Skip to main content
JulienD
Associate III
June 21, 2015
Question

STM32L1 Writing on flash works or not depending on pre-initialized values

  • June 21, 2015
  • 1 reply
  • 475 views
Posted on June 21, 2015 at 09:13

Hi,

I experiment an issue while writing data on flash.

For testing purpose, I made an app that writes several sequence of 'a' to 'z' char to

flash. Each uint_32 data contains 4 chars (a-d, e-h, ...).

I use :

HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, eeAddress, data);

I use an array to access the data :

#define EEPROM_SIZE 14 *1024

__attribute__((__section__(''.eeprom''))) uint32_t eepromZone[EEPROM_SIZE / sizeof(uint32_t)] = { value1, value2, value3 };

Everithing works fine, except for the values which are pre-initialized in the declaration.

Reading the pre-initialized values is ok.

Writing on those values gives odd results while reading.

If I initialize value1, value2 and value3 with 0, it works : I read abcdefghijklmno after writing 'abcd' in the first uint32, 'efgh' in the second, 'ijkl' in the third and 'mno' in the fourth.

If I initialize value1=0xFFFFFFFF, value2=0, value3=0, I read 0xFF FF FB FF has the first uint32, 'efgh' in the second, 'ijkl' in the third and 'mno' in the fourth after writing ''abcdefghijklmno''

If I initialize value1=0x00FFFFFF, value2=0, value3=0, I read 0x64 FF FE FF has the first uint32, 0xFFFFFFFF in the second, 'ijkl' in the third and 'mno' in the fourth after writing ''abcdefghijklmno''

If I initialize value1=0xFFFFFFFF, value2=0xFFFFFFFF, value3=0, I read 0xFFFF FB FF has the first uint32, 0xFFFFFFFF in the second, 'ijkl' in the third and 'mno' in the fourth after writing ''abcdefghijklmno''

What could happen ? What should I do to be able to pre-populated the array at flash time and modify the values after ?

If needed, here's the beginning of th ld file :

/* Entry Point */

ENTRY(Reset_Handler)

/* Highest address of the user mode stack */

_estack = 0x2000BFFF;    /* end of RAM */

/* Generate a link error if heap and stack don't fit into RAM */

_Min_Heap_Size = 0x200;      /* required amount of heap  */

_Min_Stack_Size = 0x400; /* required amount of stack */

/* Specify the memory areas */

MEMORY

{

FLASH (rx)      : ORIGIN = 0x8000000, LENGTH = 384K

RAM (xrw)      : ORIGIN = 0x20000000, LENGTH = 48K

}

/* Define output sections */

SECTIONS

{

  /* The startup code goes first into FLASH */

  .isr_vector :

  {

    . = ALIGN(4);

    KEEP(*(.isr_vector)) /* Startup code */

    . = ALIGN(4);

  } >FLASH

 .eeprom :

    {

    . = ALIGN(4);

        *(.eeprom)

    . = ALIGN(4);

    } >FLASH

 

  /* The program code and other data goes into FLASH */

  .text :

  {

    . = ALIGN(4);

    *(.text)           /* .text sections (code) */

    *(.text*)          /* .text* sections (code) */

    *(.glue_7)         /* glue arm to thumb code */

    *(.glue_7t)        /* glue thumb to arm code */

    *(.eh_frame)

    KEEP (*(.init))

    KEEP (*(.fini))

    . = ALIGN(4);

    _etext = .;        /* define a global symbols at end of code */

  } >FLASH

Thanks

Julien
    This topic has been closed for replies.

    1 reply

    JulienD
    JulienDAuthor
    Associate III
    June 22, 2015
    Posted on June 22, 2015 at 09:37

    Hum, it seems that I should erase the eeprom before writing it...