Question
STM32L1 internal temperature
Posted on August 09, 2017 at 14:44
Hello,
I use a STM32L151RCT6 on a custom board and i want to read the internal temperature.
In the cube library I found an exemple using the LL library so I included the ll_adc driver in my code and tried to use it.When I use the macro __LL_ADC_CALC_TEMPERATURE , i get a temperature of 425�C !! I know it's summer but that's a bit too hot
After some debuging, I read the calibration value at 30�C and 110�C : 668 and 846
I also read my raw adc value and get 1547So the 425�C is 'correct' regarding the calibration value but I think that the calibrations values are incorrect.
Any idea why ? and how to fix this ?
I don't need an accurate measure (5�C range will be sufficient)Brice
#stm32l1 #adc #internal-temperature-sensor