Skip to main content
LCE
Principal III
October 6, 2025
Solved

STM32L1 ADC only clocked by HSI ?

  • October 6, 2025
  • 2 replies
  • 313 views

Heyho,

just checking the L162 for a new project, then found that the ADC can only be clocked by the HSI.

Is that correct?

If yes, why?

My experience with HSI (and other RC-oscillators) is that it is "mediocre" at best, rather inaccurate and jitters like crazy. Although this might not be a big issue with a 12-bit ADC.

Merci!

This topic has been closed for replies.
Best answer by STTwo-32

Hello @LCE 

I confirm that the ADC is clocked only by HSI. For the reason behind this design choice, according to the chapter 12.3.2 of the RM0038:

"To avoid unnecessary consumption while not converting, the ADC digital interface has been designed to operate in a completely independent manner, at its maximum speed using an internal 16 MHz clock source (HSI), whatever the CPU operating frequency (which can range from a few sub-kHz up to 32 MHz)." 

Best Regards.

STTwo-32

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
October 6, 2025

Hello @LCE 

I confirm that the ADC is clocked only by HSI. For the reason behind this design choice, according to the chapter 12.3.2 of the RM0038:

"To avoid unnecessary consumption while not converting, the ADC digital interface has been designed to operate in a completely independent manner, at its maximum speed using an internal 16 MHz clock source (HSI), whatever the CPU operating frequency (which can range from a few sub-kHz up to 32 MHz)." 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LCE
LCEAuthor
Principal III
October 6, 2025

Thanks for the info.

Bad idea anyway. ;)

But probably no game stopper for my application.