Skip to main content
ren yong
Associate II
March 14, 2018
Question

STM32L073VBT6 COST 100mA,Help

Posted on March 14, 2018 at 08:09

My product with stm32l073vbt6 ran 1 week or longger,the mcu was broken.

All io and peripheral on broken mcu can run as normal,But the power consumption up to 100mA not 100uA!

I have removed all other part but mcu and supply 3.3V my own,the state  not changeï¼�

How can a mcu cost 100mA without any other chip when all function ok?

    This topic has been closed for replies.

    19 replies

    Bogdan Golab
    Lead
    March 14, 2018
    Posted on March 14, 2018 at 08:39

    Single board affected? Do you have more boards like this?

    Is the MCU hotter now? It's about 0.3W of dissipated power on small...

    Are I/O disconnected to prove that the MCU the root cause of the problem?

    Can you share the schematic? Just wonder if theoretically this amount of current is possible through I/O

    ren yong
    ren yongAuthor
    Associate II
    March 14, 2018
    Posted on March 14, 2018 at 08:52

    ALL IO float already,and I had tried connect the reset PIN to GND. It proved that the current cost internal!

    T J
    Senior III
    March 15, 2018
    Posted on March 15, 2018 at 01:10

    the circuit looks ok, you blew it up...

    there is no signs of 6V 12V in your circuit..

    what did you do ?

    sometimes a static charge blows the chip whilst it is being handled before mounting..

    this may be your issue.

    do you use Antistatic precautions ?

    ren yong
    ren yongAuthor
    Associate II
    March 15, 2018
    Posted on March 15, 2018 at 09:48

    The circuit with diff voltage all with mos or res as below.

    0690X00000604U5QAI.jpg
    henry.dick
    Associate II
    March 15, 2018
    Posted on March 15, 2018 at 03:05

    '

    How can a mcu cost 100mA without any other chip when all function ok?'

    When it is abused, damaged, or otherwise mis configured.