Skip to main content
Hattori Hanzo
Visitor II
December 4, 2018
Question

STM32L073/Unique device ID registers/unique ID bits [95:64]

  • December 4, 2018
  • 1 reply
  • 607 views

I am confused by the naming "unique ID bits" which implies that these bits are really unique from device to device.

Are these bits really unique from device to device, or are the other bits (WaferNr,LotNr [0:63]) also required to build a unique id?

This topic has been closed for replies.

1 reply

Uwe Bonnes
Chief
December 4, 2018

The whole 96 bits are unique. Byte/halfwards and words from that 96-bit number may be the same on different devices.