Skip to main content
ETone
Associate III
Apr 27, 2019 5:00 PM UTC
Question

STM32L073 system information block address map

I trying to find information on the system information block of the stm32l073rb, specifically the address of the vrefint calibration value. I've looked in the ref manual, the data sheet and the L0 HAL docs and have come up empty. Please show me how stupidly easy this is to find so I can be publicly embarrassed and flamed without mercy.

This topic has been closed for replies.

4 replies

ETone
EToneAuthor
Associate III
Apr 27, 2019 5:25 PM UTC

Whoops! wrong forum. I should be flamed. I would delete this if I could but i will repost in mcu's

Olivier GALLIEN
ST Technical Moderator
Apr 29, 2019 7:31 AM UTC

Hi,

Topics updated. No need to enter a new post.

BR,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
S.Ma
Principal
Apr 29, 2019 7:56 AM UTC

Have you checked the datasheet and ADC related electrical and memory mapping tables?

It might be next to the place talking about VTemp.

Otherwise, browse the H file defining this product registers, there might be some definitions coming from the chip spec.

Worst case a Nucleo ADC Vref example project.

Amel NASRI
ST Technical Moderator
Apr 30, 2019 9:56 AM UTC
To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.