Skip to main content
Explorer
June 12, 2025
Question

STM32L071CBT6 issue While recieving Input for GPIO pin

  • June 12, 2025
  • 1 reply
  • 253 views

 

STM32L071CBT6 GPIO PB15 Input Not Responding to 5V Signal from Buck Converter

Hello everyone,

I'm using the STM32L071CBT6 microcontroller and facing an issue with reading a digital input on GPIO pin PB15.

What I'm Trying to Do:

I’m using a buck converter with a 5V output to indicate the power status. The 5V output from the buck converter is connected to PB15, which is configured as a digital input on the STM32.

 

Setup:

  • Buck converter 5V output = GPIO PB15

  • Measured with multimeter: PB15 shows 5V when buck converter is ON

  • PB15 is configured in firmware as an input pin (floating or pull-down)

Problem:

Although PB15 is reading 5V on the pin when measured, the firmware logic that depends on PB15 being HIGH doesn't work.

 

What I’ve Checked:

  • The GPIO pin is correctly configured as input

  • Measured 5V directly at PB15

  • Tried enabling internal pull-down or external pull-down resistor

  • No response or logic change in the code when the 5V signal is applied

Why does PB15 show 5V physically (confirmed via multimeter) but the STM32L071 doesn't detect it as a logic HIGH in firmware?

This topic has been closed for replies.

1 reply

TDK
June 12, 2025

Set it as an output and drive it high and verify that (a) the voltage goes high and (b) the IDR register reflects this.

 

Related/duplicate? Just a coincidence you two asked the same uncommon question?

STM32L071CBT6 issue While recieving Input for GPIO... - STMicroelectronics Community

"If you feel a post has answered your question, please click ""Accept as Solution""."