Skip to main content
kaival
Visitor II
July 10, 2015
Question

STM32L05x not getting ACK from I2C slave.

  • July 10, 2015
  • 1 reply
  • 709 views
Posted on July 10, 2015 at 06:33

Hi

I am using STM32L05x for my project. I interfaced TLC59116 with MCU on I2C. Issue is, I can send address on but is slave is not acknowledge to the address.

Slave Address: 0xC0

I am sharing my I2C related code for reference.

static void I2c_Driver_Init(void)

{

  /*♯♯-1- Configure the I2C peripheral ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/

  I2CxHandle.Instance              = I2C1;

  I2CxHandle.Init.AddressingMode   = I2C_ADDRESSINGMODE_7BIT;

  I2CxHandle.Init.Timing           = 0x10A13E56;

  I2CxHandle.Init.DualAddressMode  = I2C_DUALADDRESS_DISABLED;

  I2CxHandle.Init.OwnAddress2Masks = I2C_OA2_NOMASK;

  I2CxHandle.Init.GeneralCallMode  = I2C_GENERALCALL_DISABLED;

  I2CxHandle.Init.NoStretchMode    = I2C_NOSTRETCH_DISABLED;

  I2CxHandle.Init.OwnAddress1      = I2C_ADDRESS;

  I2CxHandle.Init.OwnAddress2      = 0;

  if(HAL_I2C_Init(&I2CxHandle) != HAL_OK)

  {

    /* Initialization Error */

    Error_Handler();    

  } 

}

void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)

{

  GPIO_InitTypeDef GPIO_InitStruct;

  if(hi2c->Instance==I2C1)

  {

  /* USER CODE BEGIN I2C1_MspInit 0 */

  /* USER CODE END I2C1_MspInit 0 */

  

    /**I2C1 GPIO Configuration    

    PB6     ------> I2C1_SCL

    PB7     ------> I2C1_SDA 

    */

    GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;

    GPIO_InitStruct.Pull = GPIO_PULLUP;

    GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF1_I2C1;

    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

    /* Peripheral clock enable */

    __I2C1_CLK_ENABLE();

  /* Peripheral interrupt init*/

    HAL_NVIC_SetPriority(I2C1_IRQn, 0, 0);

    HAL_NVIC_EnableIRQ(I2C1_IRQn);

  /* USER CODE BEGIN I2C1_MspInit 1 */

  /* USER CODE END I2C1_MspInit 1 */

  }

}

Please let me know I am missing something?

#stm32l051x-i2c
This topic has been closed for replies.

1 reply

Amel NASRI
Technical Moderator
July 13, 2015
Posted on July 13, 2015 at 11:06

Hi shah.kaival,

In the code you shared, I don't see the call for processing functions (HAL_I2C_Master_Transmit & HAL_I2C_Master_Receive). The slave address besides to the data are transferred on the bus based on these functions.

You can take the examples available in the STM32CubeL0 package as reference.

Have a look to the ones under STM32Cube_FW_L0\Projects\STM32L053C8-Discovery\Examples\I2C. 

If the processing functions are already called on your code, try to check the acceptable address for TLC59116, is it really 0xC0?

-Mayla-

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.