Skip to main content
scc
Visitor II
May 27, 2015
Question

STM32L051C6 SPI DMA extra ghost byte

  • May 27, 2015
  • 0 replies
  • 445 views
Posted on May 27, 2015 at 15:33

Hi, 

I have discover there is one extra ghost byte is sent in SPI. I have monitor the memory area of DMA TX buffer, the data there is correct, but I will receive one extra byte in the beginning.

Here is my code

/* Buffers used for transmission */

uint8_t amsgHeadBuffer[MPUHEADERSIZE];

uint8_t amsgpayloadBuffer[MPUPAYLOADSIZE];

uint8_t aRxBuffer[BUFFERSIZE];

uint8_t aTxBuffer[BUFFERSIZE];

void spi_handler_init(void)

{

SpiHandle.Instance = SPIx;

SpiHandle.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;

SpiHandle.Init.Direction = SPI_DIRECTION_2LINES;

SpiHandle.Init.CLKPhase = SPI_PHASE_1EDGE;

SpiHandle.Init.CLKPolarity = SPI_POLARITY_LOW;

SpiHandle.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;

SpiHandle.Init.CRCPolynomial = 7;

SpiHandle.Init.DataSize = SPI_DATASIZE_8BIT;

SpiHandle.Init.FirstBit = SPI_FIRSTBIT_MSB;

SpiHandle.Init.NSS = SPI_NSS_HARD_INPUT;

SpiHandle.Init.TIMode = SPI_TIMODE_DISABLED;

SpiHandle.Init.Mode = SPI_MODE_SLAVE;

if(HAL_SPI_Init(&SpiHandle) != HAL_OK) {

/* Initialization Error */

Error_Handler();

}

if(HAL_SPI_TransmitReceive_DMA(&SpiHandle, (uint8_t *)aTxBuffer, (uint8_t *)aRxBuffer, BUFFERSIZE) != HAL_OK)

{

err = 0;

Error_Handler();

}

}

void msg_handler(void)

{

int cnt = SpiHandle.hdmarx->Instance->CNDTR;

rx_index = 0;

HAL_SPI_DMAStop(&SpiHandle);

/* 1. Get MPU Message Header */

memcpy(amsgHeadBuffer, aRxBuffer+rx_index, sizeof(MpuMsgHeader_t));

rx_index += sizeof(MpuMsgHeader_t);

msg = mpu_message_header(amsgHeadBuffer);

len_mpu_payload = msg->payloadLen;

cmd_type = msg->type;

test(msg);

if(HAL_SPI_TransmitReceive_DMA(&SpiHandle, (uint8_t *)aTxBuffer, (uint8_t *)aRxBuffer, BUFFERSIZE) != HAL_OK)

{

err = 1;

Error_Handler();

}

}

void spi_write(uint8_t * buff, int size)

{

int i;

/* pull GP_nINT_PMU_PIN low for trigger interrupt */

GP_nINT_PMU_BANK->BSRR = GP_nINT_PMU_PIN ;

udelay(50);

GP_nINT_PMU_BANK->BRR = GP_nINT_PMU_PIN ;

memset(aTxBuffer, 0x00, BUFFERSIZE);

memcpy(aTxBuffer, buff, size);

}

    This topic has been closed for replies.