Skip to main content
xle.1
Associate II
May 8, 2023 1:32 PM UTC
Solved

STM32L031K6 ISP not work

STM32 only connect VCC and UART2. Can it download programs with ISP(UART2 PA2-3)?

​

This topic has been closed for replies.
xle.1
xle.1Best answer
Associate II
May 9, 2023 3:34 PM UTC

Thanks I've solved it​

Chip failure

4 replies

waclawek.jan
Super User
May 9, 2023 11:55 AM UTC

> Can it download programs with ISP(UART2 PA2-3)?

For individual bootloader options, check AN2606.

Isn't there activity on other bootloader interfaces' pins? If yes, the bootloader may errorneously think that communication goes there.

BOOT0 is connected how? NRST is connected how?

Communication is provided how? Check using oscilloscope the waveform on the UART_Rx pin.

Does the chip work at all? Check all VDD/GND pins. Is power supply OK?

It's always better to start with a "known good" hardware e.g. a Nucleo board, which has also USB-VCP support in its on-board STLink.

JW

xle.1
xle.1Author
Associate II
May 9, 2023 3:35 PM UTC

Thanks I've solved it​

Chip failure

Tesla DeLorean
Guru
May 9, 2023 12:02 PM UTC

Show a schematic.

If analogue supply pins, make sure they are wired too.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
xle.1
xle.1AuthorBest answer
Associate II
May 9, 2023 3:34 PM UTC

Thanks I've solved it​

Chip failure