Skip to main content
Mads Enevoldsen
Associate
Feb 28, 2017 3:22 PM UTC
Solved

STM32L031 program does not run.

Posted on February 28, 2017 at 16:22

1:

I have developed a small program for the STM32L031 Nucleo-32 using the example UART_TwoBoards_ComIT. The program run on the STM32L031 Nucleo-32 develop-board. When I load* the program to our own HW it does not start, I have tried with and without the compiler directive USE_STM32L0XX_NUCLEO_32. I suspect the system clock generation, but can’t find where it is setup.

*I load the program using STM flash_loader_demo_v2.8.0.

2:

I want to use the ST-LINK V2 for debug should the data port be connected to PA13?

Do any have a hint or comments that could help me?

-Mads

    This topic has been closed for replies.
    Mads Enevoldsen
    Mads EnevoldsenBest answer
    Associate
    Mar 2, 2017 8:48 AM UTC
    Posted on March 02, 2017 at 08:48

    Hi Clive

    FYI

    1: I forced the program to use the HSE clock now it works.

    2 The TDO_SWO is optional now the bugger also works.

    Problems solved!

    -Mads

    6 replies

    Tesla DeLorean
    Guru
    Feb 28, 2017 3:36 PM UTC
    Posted on February 28, 2017 at 16:36

    You would need to connect both SWDIO (PA13) and SWCLK (PA14), VCC and GND would also need connections to the ST-LINK. The connection of NRST would also be desirable.

    Make sure BOOT0 pin is pulled low to execute your code.

    Then use a debugger to understand what is happening, or GPIO/USART signalling

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Max
    ST Employee
    Mar 1, 2017 4:45 AM UTC
    Posted on March 01, 2017 at 05:45

    There is already a STLink V2-1 embeded on the 

    STM32L031 Nucleo-32 (on the bottom side of the PCB) and it is already properly connected unless you (removed some 0 Ohms resistors).

    Check

    http://www.st.com/content/ccc/resource/technical/document/user_manual/1b/03/1b/b4/88/20/4e/cd/DM00105928.pdf/files/DM00105928.pdf/jcr:content/translations/en.DM00105928.pdf

    and

    http://www.st.com/content/ccc/resource/technical/document/user_manual/e3/0e/88/05/e8/74/43/a0/DM00231744.pdf/files/DM00231744.pdf/jcr:content/translations/en.DM00231744.pdf

    , you will get a lot of useful information
    Tesla DeLorean
    Guru
    Mar 1, 2017 5:56 AM UTC
    Posted on March 01, 2017 at 05:56

    >>

    When I load* the program to our own HW it does not start

    Emphasis mine, the OP is discussing two situations, a working Nucleo, and a non-working custom board needing connectivity to an ST-LINK to debug the situation.

    The Nucleo will have an 8 MHz clock source feed from the onboard ST-LINK. This is likely not present on the custom board, so BYPASS mode won't work, and HSE must start succesfully. Settings in SystemInit() need review.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Mads Enevoldsen
    Associate
    Mar 1, 2017 10:13 AM UTC
    Posted on March 01, 2017 at 10:13

    Hi Clive

    I understand I can't use the SWIM connector, but what about TDO_SWO connection?

    ST-LINK/V2

    connector

    (CN3)

    ST-LINK/V2 function

    Target connection

    (JTAG)

    Target connection

    (SWD)

    STM32L031

    1,2

    VAPP

    Target VCC

    MCU VDD(1)

    MCU VDD(1)

    VDD

    3

    TRST

    JTAG TRST

    JNTRST

    GND(2)

    GND

    4

    GND

    GND

    GND(3)

    GND(3)

    GND

    5

    TDI

    JTAG TDO

    JTDI

    GND(3)

    GND

    6

    GND

    GND

    GND(3)

    GND(3)

    GND

    7

    TMS_SWDIO

    JTAG TMS, SW IO

    JTMS

    SWDIO

    PA13

    8

    GND

    GND

    GND(3)

    GND(3)

    GND

    9

    TCK_SWCLK

    JTAG TCK, SW CLK

    JTCK

    SWCLK

    PA14

    10

    GND

    GND

    GND(3)

    GND(3)

    GND

    11

    NC

    Not connected

    Not connected

    Not connected

    NC

    12

    GND

    GND

    GND(3)

    GND(3)

    GND

    13

    TDO_SWO

    JTAG TDI, SWO

    JTDO

    TRACESWO(4)

    ?

    14

    GND

    GND

    GND(3)

    GND(3)

    GND

    15

    NRST

    NRST

    NRST

    NRST

    NRST

    16

    GND

    GND

    GND(3)

    GND(3)

    GND

    17

    NC

    Not connected

    Not connected

    Not connected

    NC

    18

    GND

    GND

    GND(3)

    GND(3)

    GND

    19

    VDD

    VDD (3.3V) (5)

    Not connected

    Not connected

    NC

    20

    GND

    GND

    GND(3)

    GND(3)

    GND

    -Mads