Skip to main content
LCE
Principal III
Mar 18, 2025 3:57 PM UTC
Solved

STM32L031 noisy, even in reset - EDIT: it's not the STM32

EDIT: it's not the STM32, see latest post

Heyho,

I have some custom miniature PCBs here, the unholy combination of a super-high-impedance-low-noise amplifier (going to a low noise audio input with 24bit ADC, spectra below from that one) and a STM32L031 on another PCB.

Both circuits share the same ground and power supply.

Actually, I didn't expect the analog part to be that good (shielding issues), so I was greatly annoyed when all got worse when adding the PCB with the MCU.

I already got the noise down by not using the CPU sleep mode: the timer interrupt frequency of 10 kHz was clearly visible in the spectrum, seemingly due to powering the CPU up and down.

Now the noise doesn't change, no matter which peripherals I turn on or off - and even in hardware reset (NRST grounded) there are the same noise spikes at around 4 kHz (and harmonics) on the analog signal.

Noise is only about -80 dBV = 100 µV, but I'd like to find out where that comes from - even with the MCU in reset.

Here are some screenshots with time signal and spectrum:

Amp_Noise_MCU_removed.png

LCE_0-1742313100646.png

 

LCE_1-1742313120753.png

 

Notes:
- ground loops removed (the signal looks much worse with non-isolated UART or ST-Link)
- I'm pretty sure it's NOT aliasing from the audio ADC (good analog AA filter and a stopband attenuation of 116dB)

Any ideas ? What could cause these 4 kHz ?

Thanks in advance!

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Mar 18, 2025 8:59 PM UTC

This is probably an artefact coming from the L0's internal power supply. Is not a plain LDO, rather, is something relatively complex using switching capacitors. It has been discussed here in the past, with ST contribution, but I don't have a link, sorry; and also I don't think there was any remedy offered, probably just the above facts were stated.

In other words, treat the 'L0 as a switching circuit, generating current pulses at its input.

JW

9 replies

LCE
LCEAuthor
Principal III
Mar 18, 2025 4:14 PM UTC

I forgot to mention:

  • I checked the ref manual (RM0377, table 34 and text), that shows that all clocks should be off with NRST = 0
  • I removed all other active components from the MCU PCB
  • I checked the 3.3V LDO with several loads (also way above what the MCU might draw), all quiet

 

waclawek.jan
waclawek.janBest answer
Super User
Mar 18, 2025 8:59 PM UTC

This is probably an artefact coming from the L0's internal power supply. Is not a plain LDO, rather, is something relatively complex using switching capacitors. It has been discussed here in the past, with ST contribution, but I don't have a link, sorry; and also I don't think there was any remedy offered, probably just the above facts were stated.

In other words, treat the 'L0 as a switching circuit, generating current pulses at its input.

JW

LCE
LCEAuthor
Principal III
Mar 19, 2025 6:36 AM UTC

Wait, what, so there's probably a switched capacitor regulator instead of a linear regulator? Oh my...

Thanks a lot @waclawek.jan !

Especially the noise with the MCU in reset really drove me crazy, made me look for some resonance within my power supply or in other parts of the circuit.

@Peter BENSCH or @STea or any other ST person:

1) This should be documented somewhere in the DS and / or RM, or is it? If yes, where?

2) This is for a soon-to-be-released product, any alternatives? 

The MCU I need must have:

  • internal EEPROM
  • 12bit ADC (with inbuilt oversampler would be nice) with DMA
  • small package that can be soldered manually (no BGA or WLCSP), right now it's QFN28 4x4 which is actually the limit space-wise

Otherwise it'll be ATmega again...

Ozone
Principal
Mar 19, 2025 7:20 AM UTC

> Wait, what, so there's probably a switched capacitor regulator instead of a linear regulator? Oh my...

Switched capacitors are e.g. used to generate the voltages required for flashing (erase & write), which are in the range of 9 to 12V.
Perhaps this block is idling here ?

> The MCU I need must have: ...

I would choose a variant with separate analog power supply.
Several STM32 MCUs do have that.

waclawek.jan
Super User
Mar 21, 2025 9:41 AM UTC

@Ozone,

No, the 'L0 appears to have switched capacitor power supply in place of the "main" LDO, generating core voltage.

@LCE,

"EEPROM" (portion of FLASH which is reprogrammable in relatively small chunks - words if I remember correctly) is unique to 'L1 (which you don't want to use, as they are rather bit, old and going to be obsolete quite soon) and 'L0. In other families, you would need to simulate EEPROM-like behaviour in larger sector(s) ("erase units"), or use an external EEPROM chip.

At this stage, you may perhaps want to consider redesigning the power supply to be able to better absorb the pulsing consumption (basically just trying various different LDOs), or decoupling the mcu from the sensitive analog e.g. by a choke (LC filter) or using two separate LDOs.

JW

Ozone
Principal
Mar 21, 2025 10:28 AM UTC

> No, the 'L0 appears to have switched capacitor power supply in place of the "main" LDO, generating core voltage.

This might well be, I have no special knowledge of such internal details.

However, the main advantage of switched capacitors is IMHO creating output voltage greater than V(in) without coils, and thus suitable for silicon implementation. Just saying ...

 

LCE
LCEAuthor
Principal III
May 6, 2025 11:19 AM UTC

My apologies to ST and the nice people who took their time to help.

I forgot about one other active component on the PCB: a small hall-switch is the culprit.
And that one also has a sleep cycle to save power, and this caused the noise.

I found that a few weeks ago, but I forgot about the thread here.

I re-designed the power supply to the hall-switch and the layout, and chose another hall-switch.
Now there's only some low frequency noise in the signal, no significant peaks anymore.

waclawek.jan
Super User
May 6, 2025 11:48 AM UTC

Thanks for coming back with the solution. A good reminder that todays ICs are very complicated and yes, they may exhibit surprising current consumption patterns at times.

At this point, you may want to unmark my post above and mark yours as the real solution.

JW

LCE
LCEAuthor
Principal III
May 6, 2025 12:25 PM UTC

I thought about unmarking the solution, but I think it's a good info that the L0-series uses some internal power switching, so I'd like to keep it.