Skip to main content
Associate II
August 26, 2025
Solved

STM32L011U USART DMA1_Channel3 not work,but DMA1_Channel5 work

void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(huart->Instance==USART2)
{
/* USER CODE BEGIN USART2_MspInit 0 */

/* USER CODE END USART2_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_USART2_CLK_ENABLE();

__HAL_RCC_GPIOB_CLK_ENABLE();
/**USART2 GPIO Configuration
PB6 ------> USART2_TX
PB7 ------> USART2_RX
*/
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF0_USART2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

/* USART2 DMA Init */
/* USART2_RX Init */
hdma_usart2_rx.Instance = DMA1_Channel3;// DMA1_Channel5 work 
hdma_usart2_rx.Init.Request = DMA_REQUEST_4;
hdma_usart2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_usart2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_usart2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_usart2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_usart2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_usart2_rx.Init.Mode = DMA_NORMAL;
hdma_usart2_rx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
if (HAL_DMA_Init(&hdma_usart2_rx) != HAL_OK)
{
Error_Handler();
}

__HAL_LINKDMA(huart,hdmarx,hdma_usart2_rx);

/* USART2 interrupt Init */
HAL_NVIC_SetPriority(USART2_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(USART2_IRQn);
/* USER CODE BEGIN USART2_MspInit 1 */

/* USER CODE END USART2_MspInit 1 */
}

} 



void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)
{
//recv size
uint8_t send_buf[2];
send_buf[0]=Size&0xFF;
send_buf[1]=Size>>8;
HAL_UART_Transmit(huart,send_buf,2,20);
HAL_UARTEx_ReceiveToIdle_DMA(&huart2,buf,32);
}

int main(void)
{
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */

 HAL_UARTEx_ReceiveToIdle_DMA(&huart2,buf,32);//start recv
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

Edited by ST Moderator to apply source code formatting - please see this guideline How to insert source code.

 

 

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
August 29, 2025

Hi @ElectronicABC ,

Did you solve this issue ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

ST Technical Moderator
August 26, 2025

Hello @ElectronicABC,

When USART2 uses DMA channel 3 for data reception, data transfers are blocked after the first byte has been
received. As a result, DMA channel 3 cannot be used for USART2 data reception.

This is mentioned in the STM32L011x3 errata sheet:

"

2.11.6 DMA channel 3 (CH3) not functional when USART2_RX used for data reception
Description
When USART2 uses DMA channel 3 for data reception, data transfers are blocked after the first byte has been
received. As a result, DMA channel 3 cannot be used for USART2 data reception.
Workaround
Use DMA channel 5 (CH5) for USART2 data reception.

"

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
August 29, 2025

Hi @ElectronicABC ,

Did you solve this issue ?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate II
August 29, 2025

yes,solve the issue,tks.