STM32L0 RTC AlarmA - set to interrupt at the desired HRS and MINUTES setting
I have working code for an STM32L0 device that uses Alarm A of the RTC to wake / interrupt at the desired minute interval. I now require the ability to wake / interrupt at the desired hours AND minutes time. Previously all masks were masked except for the Alarm A minutes mask. Now all masks except for the Alarm A minutes AND hours masks are masked. I believe it should work as before only now the alarm needs to see a matching hours AND minutes value in order to cause the interrup. Is my understanding correct ? So, for example, if the current time is 0 hrs and 0 minutes and I set AlarmTime.Hours = 1 and AlarmTime.Minutes = 1 then I would expect a single interrupt 61 minutes from now.