Question
STM32L0 MCU EEPROM write
Posted on July 29, 2014 at 14:44
Hi.
I use Nucleo board with STM32L0x3 MCU. There are special sequence for EEPROM TYPEPROGRAM_BYTE process?
I can write 4 bytes data (TYPEPROGRAM_WORD) but can't write 1 byte data (TYPEPROGRAM_BYTE):uint32_t
Address = 0;uint32_t
data32 = 0x12345678;uint8_t
ubData[10] = {0};// write 4 bytes example - work
while
(Address < FLASH_USER_END_ADDR){
if
(HAL_DATA_EEPROMEx_Program(TYPEPROGRAM_WORD, Address, data32) == HAL_OK){
Address = Address + 4;
}
else
{
Error_Handler();
}
i -= 4;
}
// write
1
byte example –does not work
while
(i > 0){
if
(HAL_DATA_EEPROMEx_Program(TYPEPROGRAM_BYTE, Address, ubData[i]) == HAL_OK){
Address = Address + 1;
}
else
{
Error_Handler();
}
i -= 1;
}
Thanks.