STM32L0 - How do I now how much time the board stayed in standby mode?
I'm working with the SMT32l072 and in my application the board runs the main routine them it stays in standby until the RTC Timer (5 minutes) or the RTC Tamper detection (A sensor that pulls down the pin) wakes the board. The thing is that when the board wakes by the tamper I need, after processes some data, to put it back to sleep for the remaining time in the RTC Wake up timer. But I can't figure out how to do it, Anyone can give me a hand?