Skip to main content
laurent1
Associate
September 21, 2017
Question

STM32L0 Cannot wakeup from STOP with LPTIM IRQ ?

  • September 21, 2017
  • 1 reply
  • 736 views
Posted on September 21, 2017 at 13:00

Hello,

I'm trying to wake up from STOP mode using LPTIMer on STM32L

LPTIM is clocked by LSE(32K) used as a simple upcounter, and I'm using both ARR and CMP Interrupts from LPTIM, so corresponding bits are set in LPTIM1->IER and NVIC->ISER.

For the purpose of using it in low-power modes I did the following extra steps:

- set LPTIM1SMEN bit in RCC->APB1SMENR

- set EXTI_IMR_IM29 in EXTI->IMR that should let EXTI29/LPTIM IRQ generate a wakeup from STOP event.

It works fine in various sleep modes unless I go to STOP (SLEEPDEEP bit in SCB->SCR) where I stay stuck.

I looked into STM32Cube examples (LPTIM_Timeout,LPTIM_PWM_LSE) and I did not find a clue.

Strangely enough, functions like HAL_LPTIM_Counter_Start_IT even write in bits that doesn't exist in the reference manual like bit 29 of EXTI->RTSR or FTSR... Of course I gave it a try, but without results.

So am I missing something ?

Best regards,

Laurent

#stm32-stm32l0 #low-power #wake-up-from-stop-mode #lptim
This topic has been closed for replies.

1 reply

joshua.cowpland
Associate II
February 4, 2019

Did you ever get this working?