Skip to main content
hartmann
Associate
October 10, 2012
Question

STM32L temperature trimming values 90° or 110°

Posted on October 10, 2012 at 09:25

Hello,

currently I'm evaluating the internal temperature senor of the STM32L151, but in the docs are different values for trimming values given. Sometimes 90° is stated somtimes 110°, so which value is correct?

STM32L151xx datasheet -> 110° for upper factory trimming value

STM32L151xx errata     ->    90°

RM0038 reference manual -> 90°

regards

thomas
    This topic has been closed for replies.

    3 replies

    raptorhal2
    Lead
    October 10, 2012
    Posted on October 10, 2012 at 16:05

    In fact it doesn't matter. The relevant advice from the user manual is:

    To reduce the temperature sensor error, the user can measure it at ambient temperature

     

    (25°C) to redefine more accurately the average slope (avg_slope) and the offset.

    The temperature sensor has an offset that varies from one processor to another, so each processor needs to be calibrated.

    If your design is for a production run, an external temperature sensor with less variation in offset might be more suitable.

    Cheers, Hal

    sheldon
    Associate
    October 15, 2012
    Posted on October 16, 2012 at 01:54

    I just received an email from ST stating:

    I have preliminary information from our factory, and it appears STM32Ls high density such as yours have correctly programmed engineering data only starting from revision Y (newer than your revision Z).

    All previous revisions are susceptible to bad engineering data programming.

    (I'm using STM32L152VC)

    raptorhal2
    Lead
    October 16, 2012
    Posted on October 16, 2012 at 15:28

    Now we just have to figure out the algorithm difference between ''

    correctly programmed engineering data

    '' and

    ''bad engineering data programming''.

    STOne - What is the design slope and offset for Revision Z ? Is there a way that Revision C can be used to measure internal temperature ?

    If all else fails, with Rev C use actual readings with the processor in a plastic bag in ice water, then at room temperature, then in your expected usage environment with a thermometer nearby. For production, you should switch to Rev Z.

    Cheers, Hal