Skip to main content
yves2399
Associate
May 14, 2013
Question

STM32L discovery I can not load program from Keil

  • May 14, 2013
  • 1 reply
  • 456 views
Posted on May 14, 2013 at 17:31

I have 3 STM32L152 discovery which anser ''Unknown target connected'' when I load a program from keil.

I try  setting BOOT0 HIGH when I push the  reset Button .

There no result.

Best regards

Yves de Brest

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    May 14, 2013
    Posted on May 14, 2013 at 18:11

    Make sure you've configured the Debugger to use SWD mode.

    Ensure you have current drivers and firmware. Confirm connectivity/function with the ST-Link Utilities.

    The older firmware will expect you to use the ''ST-Link (Deprecated Version)'' connection in Keil. The newer firmware ''ST-Link Debugger''

    There have classically be download issue with Keil/ST-Link (Flash->Download), but the debug/download option should work.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..