Skip to main content
Krenek.Steve
Associate II
July 7, 2013
Question

STM32L clock battery backup

  • July 7, 2013
  • 3 replies
  • 715 views
Posted on July 07, 2013 at 22:56

The STM32L series does no have a dedicated pin for a battery backup to keep the RTC running when the supply is removed.

What is the recommended way to provide battery backup of the RTC for this series?

#rtc #battery-backup-stm32l
This topic has been closed for replies.

3 replies

jpeacock2399
Associate III
July 7, 2013
Posted on July 07, 2013 at 23:13

Look at the VBAT pin.  It's used to power the backup domain, including RTC and backup SRAM memory.  It works with a battery or supercap.

  Jack Peacock
Tesla DeLorean
Guru
July 7, 2013
Posted on July 07, 2013 at 23:56

The L series parts are designed to run from a battery, if you expect the device to keep running you're going to need to supply a voltage all the time, either by powering it by a battery with a charger circuit behind it, or split a permanent/temporal supply via some diodes, like a

http://www.nxp.com/products/diodes/switching_diodes/BAV70.html%3bjsessionid=540DB166652B4BAC6B0011DF38BE52CC?CTV=googlesem_GA_R33_BAV70&cid=prod_discretes-web_advertising_search-01_01_13

, or something along those lines.

The use of a 32.768 KHz crystal is also recommended, I think you can use other clocks in the L, but all the other STM32 series only have this clock in the backup domain.

No VBAT pin on STM32L1xx parts BTW

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
tech2
Visitor II
March 26, 2015
Posted on March 26, 2015 at 12:35

Sorry, my mistake.