Skip to main content
Associate II
July 6, 2024
Question

STM32H7xx USART3 can't wake up from STOP mode

Our product uses a STM32H7xx chip, integrate freeRTOS. We want our product can go into STOP mode to save power, and can be waked up from STOP by USART3 receiving data.

Below is some related code, but it does not work, our product can't be waked up by USART data. 

 

MX_USART3_UART_Init is generated by CubeMx, we just add a few code at the beginning and end to config WUS clock and IT.

void MX_USART3_UART_Init(void)
{
/* USER CODE BEGIN USART3_Init 0 */
__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_HSI);
/* USER CODE END USART3_Init 0 */

/* USER CODE BEGIN USART3_Init 1 */

/* USER CODE END USART3_Init 1 */
huart3.Instance = USART3;
huart3.Init.BaudRate = 115200;
huart3.Init.WordLength = UART_WORDLENGTH_8B;
huart3.Init.StopBits = UART_STOPBITS_1;
huart3.Init.Parity = UART_PARITY_NONE;
huart3.Init.Mode = UART_MODE_TX_RX;
huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart3.Init.OverSampling = UART_OVERSAMPLING_16;
huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart3) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_2) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_2) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_EnableFifoMode(&huart3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART3_Init 2 */
__HAL_UART_ENABLE_IT(&huart3, UART_IT_RXNE);
__HAL_UART_ENABLE_IT(&huart3, UART_IT_WUF);
/* USER CODE END USART3_Init 2 */
}

 

Below is our code to go into STOP mode and wake up in one freeRTOS task.

HAL_SuspendTick();
HAL_UARTEx_EnableStopMode(&huart3);
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

HAL_ResumeTick();
SystemClock_Config();

This topic has been closed for replies.

1 reply

ST Employee
July 15, 2024

Hello @HarryXia 

There is an example in CubeH7 using UART wakeup from stop mode using FIFO: 

STM32CubeH7/Projects/STM32H747I-DISCO/Examples/UART/UART_WakeUpFromStopUsingFIFO at master · STMicroelectronics/STM32CubeH7 · GitHub

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.