Skip to main content
Hartmut Meyer
Associate
Jan 28, 2018 3:09 PM UTC
Solved

STM32H7xx Example-programs

Posted on January 28, 2018 at 16:09

I am using the STM32H743 together with uVision 5.

Are there any example-programs available not using RTOS2 and CubeMX ?

What I am missing are simple demo-programs like Blinky ( without RTX ) and a demo-program

using the LCD ( without a GUI, yust a simple output of text would be fine ).

I have available a project, the only purpose shall be to switch an LED on,

it compiles, links and flashes without error, but nothing else happens...

Probably an initialisation-problem but I need a working example to get on the right path.

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Jan 28, 2018 4:16 PM UTC
    Posted on January 28, 2018 at 17:16

    Outputting text isn't exactly simple, you have to paint the bitmaps

    HAL examples are under the Cube Repository trees

    \STM32Cube_FW_H7_V1.1.0\Projects\STM32H743I_EVAL\Examples\GPIO\GPIO_EXTI\Src\main.c

    \STM32Cube_FW_H7_V1.1.0\Projects\STM32H743I_EVAL\Examples\UART\UART_Printf

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    4 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Jan 28, 2018 4:16 PM UTC
    Posted on January 28, 2018 at 17:16

    Outputting text isn't exactly simple, you have to paint the bitmaps

    HAL examples are under the Cube Repository trees

    \STM32Cube_FW_H7_V1.1.0\Projects\STM32H743I_EVAL\Examples\GPIO\GPIO_EXTI\Src\main.c

    \STM32Cube_FW_H7_V1.1.0\Projects\STM32H743I_EVAL\Examples\UART\UART_Printf

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Joerg Wagner
    Senior III
    Jan 28, 2018 5:21 PM UTC
    Posted on January 28, 2018 at 18:21

    Custom or ST board?

    In case of Nucleo or Eval, which LED did you try turn on?

    Tesla DeLorean
    Guru
    Jan 28, 2018 8:51 PM UTC
    Posted on January 28, 2018 at 20:51

    The availability of an LCD suggests the STM32H743I-EVAL, and ST doesn't provide examples for third party boards.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Hartmut Meyer
    Associate
    Jan 29, 2018 8:23 AM UTC
    Posted on January 29, 2018 at 09:23

    There are already excellent examples available inside the STM32Cube-firmware-package,

    Uefull as well for Keils MDK-toolchain.

    I only haven't expected to find them there at first.