Skip to main content
Associate III
Sep 26, 2025 10:08 AM UTC
Solved

STM32H7S78-DK: How to determine VOS0, VOS1, VOS2 and VCore for estimating lifetime

Hello,

according to this document 

https://www.st.com/resource/en/application_note/an5337-guidelines-for-estimating-stm32h7-mcus-lifetime-stmicroelectronics.pdf

the expected lifetime of a STM32H7 mcu depends on the parameters Tj (junction temperature), VOS0, VOS1, VOS2, VCore and operation ratio.

How can we determine VOS0, VOS1, VOS2 and VCore for the STM32H7S78-DK board?

 

Thanks in advance,

rk_iot

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Oct 22, 2025 11:05 AM UTC

Hello @rk_iot 

Please forget about the previous tables. This is an updated estimated lifetime table for H7RS no matter the mission profile is:

H7RS_lifetime.png

AN5337 will be updated in 2026. We don't have the exact deadline at the moment.

Hope that it answers you question. 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

12 replies

AScha.3
Super User
Sep 26, 2025 10:35 AM UTC

> How can we determine

Just your decision, you select the vosx you want.

And so you also fix the frequency the CPU is working on and this way also the current consumption and the lifetime.

Depends on expected max ambient temperature...and your decisions.

If you feel a post has answered your question, please click on " Best Answer ".
rk_iotAuthor
Associate III
Sep 26, 2025 11:26 AM UTC

Thank you @AScha.3 !

So when running the CPU with 600 MHz, what will be the values for VOS0, VOS1, VOS2 and VCore?

We could not find these values in the reference manual:

https://www.st.com/resource/en/reference_manual/rm0477-stm32h7rx7sx-armbased-32bit-mcus-stmicroelectronics.pdf

 

Thank you and best regards,

rk_iot

mƎALLEm
ST Technical Moderator
Sep 26, 2025 11:52 AM UTC

@rk_iot wrote:

Thank you @AScha.3 !

So when running the CPU with 600 MHz, what will be the values for VOS0, VOS1, VOS2 and VCore?

We could not find these values in the reference manual:

https://www.st.com/resource/en/reference_manual/rm0477-stm32h7rx7sx-armbased-32bit-mcus-stmicroelectronics.pdf

 

Thank you and best regards,

rk_iot


This kind of information can be found in the datasheet but seems only two voltage levels are available (low and high)

mALLEm_0-1758887474514.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
rk_iotAuthor
Associate III
Sep 26, 2025 12:15 PM UTC

Thank you @mƎALLEm and @AScha.3 

 

our confusion probably stems from the fact that AN5337 is not intended for STM32H7R7/7S7.

It says it is only applicable for:

STM32H742, STM32H743/753, STM32H745/755, STM32H747/757, STM32H750 Value line
STM32H723/733, STM32H725/735, STM32H730 Value line

Is there a corresponding document for STM32H7R7/7S7?

We would need a way to reliably determine the life time expectancy for our application. Maybe it is enough to measure the temperature on the chip surface and know the core voltage and core frequency to get an good estimation?

 

Thank you and best regards,

rk_iot

 

mƎALLEm
ST Technical Moderator
Sep 26, 2025 1:36 PM UTC

@rk_iot wrote:

Is there a corresponding document for STM32H7R7/7S7?


There is no document for STM32H7R7/7S7 devices but the plan is to update the AN5337. I don't know when it will be updated.

But according to what I found internally as information:
The estimation of the current profile is given in the Table below. 

mALLEm_0-1758893672460.png

The target for the industrial mission profile is given below also.
Estimated lifetime @ Operating ratio 100%

mALLEm_1-1758893685481.png

Hope that helps.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
rk_iotAuthor
Associate III
Sep 29, 2025 7:36 AM UTC

Hello @mƎALLEm ,

thank you for that helpful information!

What exactly is the difference between the first and the second table? What does "industrial mission profile" mean?

Our guess is that the first table is for STM32H7S7L8H6 and the second "industrial mission profile" table is for STM32H7S7L8H6H?

But we could not find that information on the product page or datasheet. Can you tell us where to find the differences between STM32H7S7L8H6  and STM32H7S7L8H6H?

Thank you and best regards

rk_iot

mƎALLEm
ST Technical Moderator
Sep 29, 2025 9:42 AM UTC

@rk_iot wrote:

Hello @mƎALLEm ,

Our guess is that the first table is for STM32H7S7L8H6 and the second "industrial mission profile" table is for STM32H7S7L8H6H?


No the H prefix in that situation means the availability of the HexaSPI interface: H6H: HexaSPI is available / H6: HexaSPI is not available.

I'm not expert of lifetime/profile subject but it's up to you to define which profile you decide to use based on your application, its usage and its environment.

For example, if your product in a harsh environment in which TJ should reach 130°c , you should use VOS low/400MHz and the lifetime will be 10 years.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
rk_iotAuthor
Associate III
Sep 29, 2025 9:58 AM UTC

@mƎALLEm but the first table says 

10 years with VOS high and Tj=55°C

and the second table

10 years with VOS high and Tj=74.3°C

what is the difference between the two tables if it is not the grade of the chip? How is "industrial mission profile" defined in that context?