Skip to main content
Associate II
August 13, 2025
Question

STM32H7B3 continously resetting when executing code from external flash

  • August 13, 2025
  • 6 replies
  • 635 views

We have a working production firmware for the STM32H7B3 that uses a Winbond W25Q01JVZEIM external flash using QSPI in memory-mapped mode to store data and assets for a TouchGFX and other applications.

Now, due to internal flash limitations, we are attempting to execute some code directly from the same external flash. As a starting point, we created a simple test function to run from external flash:

__attribute__((section("ExtFlashSection")))

void test_ext_flash_func(void) {

 volatile int x = 1;

 x++;

}

The rest of the application continues to run from internal flash. However, when this function is called, the MCU enters a continuous reboot loop. We have added Hard fault handler but couldn't see any prints for different register values.

Current Configuration

  1. Linker Script
MEMORY

{

 ...

 OSPI (xr) : ORIGIN = 0x93170000, LENGTH = 32M

}



SECTIONS

{

 ...

 ExtFlashSection :

 {

 *(ExtFlashSection ExtFlashSection.*)

 *(.gnu.linkonce.r.*)

 . = ALIGN(0x4);

 } > OSPI

}

2. MPU Configuration

I have added this now for getting the code to execute from external flash based on some online documentation that I saw. This wasn't present in our earlier implementation.

void MPU_Config(void)

{

 // Disable MPU

 MPU->CTRL &= ~MPU_CTRL_ENABLE_Msk;



 // Configure Region 0 for QSPI external flash

 MPU->RNR = 0; // Select Region 0

 MPU->RBAR = 0x93170000; // Base address of QSPI flash



 // Region size = 32MB → log2(32MB) = 25 → 0x19 << 1 = 0x32

 MPU->RASR = (0x19 << MPU_RASR_SIZE_Pos) | // Size = 32MB

 (0 << MPU_RASR_TEX_Pos) | // TEX = 0

 (1 << MPU_RASR_C_Pos) | // Cacheable

 (0 << MPU_RASR_B_Pos) | // Not bufferable

 (0 << MPU_RASR_S_Pos) | // Not shareable

 (3 << MPU_RASR_AP_Pos) | // Full access

 (0 << MPU_RASR_XN_Pos) | // Executable

 (1 << MPU_RASR_ENABLE_Pos); // Enable region



 // Enable MPU with default memory map for privileged access

 MPU->CTRL = MPU_CTRL_ENABLE_Msk | MPU_CTRL_PRIVDEFENA_Msk;



 // Ensure MPU settings take effect

 __DSB();

 __ISB();

}

3. OCTOSPI Driver Initialization

static void enableMemoryMappedMode( void ) // QPI mode only

{

 OCTOSPI1->CR &= (~(OCTOSPI_CR_FMODE | OCTOSPI_CR_FTHRES));

 OCTOSPI1->CR |= (OCTOSPI_CR_FMODE_1 | OCTOSPI_CR_FMODE_0);

 OCTOSPI1->CCR = OSPI_COMM_CFG_CMD_ADDR_DATA;

 OCTOSPI1->TCR = (FLASH_CFG_QPI_NO_OF_DUMMY_CLK << OCTOSPI_TCR_DCYC_Pos) | OCTOSPI_TCR_SSHIFT;

 OCTOSPI1->IR = FLASH_CMD_FAST_READ_QPI;

}

OSPIDriverinit()

{

flashSendCMDNoData( FLASH_CMD_ENABLE_4B_ADDR_WB, true ); // Enable the 4 byte addressing mode for all commands

 flashReadChipData( FLASH_CMD_READ_SR2_REG_WB, &tmpSRData.statusReg2, 1, 0, true );

 if( (tmpSRData.statusReg2 & FLASH_SR2_QE_MASK_WB) == 0 )

 {

 tmpSRData.statusReg2 |= FLASH_SR2_QE_MASK_WB;

 flashSendCMDNoData( FLASH_CMD_WRITE_ENABLE, true );

 flashWriteChipData( FLASH_CMD_WRITE_SR2_REG_WB, &tmpSRData.statusReg2, 1, true );

 do

 {

 flashReadChipData( FLASH_CMD_READ_SR1, &tmpSRData.statusReg1, 1, 0, true );

 } while( (tmpSRData.statusReg1 & FLASH_SR1_BUSY) != 0 );

 }

 // Enable QPI mode

 flashSendCMDNoData( FLASH_CMD_ENABLE_QPI_WB, true );

 // Configure the number of dummy cycles for 100 MHz operation

 tmpData = FLASH_CFG_QPI_RD_CFG_REG_WB;

 flashWriteChipData( FLASH_CMD_WRITE_RD_CFG_WB, &tmpData, 1, false );

 selectedDie = 0;

 isDualDieStatReg = true;

 flashWriteChipData( FLASH_CMD_SELECT_DIE_WB, &selectedDie, 1, false );

 }

__NVIC_DisableIRQ( OCTOSPI1_IRQn );

 __NVIC_SetPriority( OCTOSPI1_IRQn, OCTOSPI1_PRIO );

 enableMemoryMappedMode();

}

4. Main Function

int main(void){

SystemClockConfig();

 MPU_Config();

 // Enable I-Cache

 SCB_EnableICache();

 // Enable D-Cache

 SCB_EnableDCache();

....

OSPIDriverinit()

....

test_ext_flash_func() // Inside a thread

….

}

Issue

Calling test_ext_flash_func() causes the MCU to reboot continuously. We suspect this is due to executing code from external flash, but need help identifying the root cause and resolving it.

This topic has been closed for replies.

6 replies

unsigned_char_array
Lead III
August 13, 2025
"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
ST Employee
August 14, 2025

Hello @devanshu5,

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

Best regards,
Maxime

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
devanshu5Author
Associate II
August 18, 2025

Hi Team,

Please help with the analysis of this issue as soon as possible. It is blocking us from moving ahead.

Regards,

Devanshu Agarwal

Tesla DeLorean
Guru
September 9, 2025

Is it generating a physical reset via NRST pin? Can you monitor that? What's the periodicity?

Do you have a Watchdog running?

Do you have a Hard Fault Handler?

Anything calling NVIC_SystemReset() or equivalent?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
devanshu5Author
Associate II
September 10, 2025

We were able to resolve this issue. No further support required for now.

unsigned_char_array
Lead III
September 10, 2025

What was the cause?

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."