Skip to main content
Associate III
Dec 24, 2025 7:04 AM UTC
Solved

STM32H7A3AII6Q Internal bootloader boot for firmware update.

Hello,

    I'm working into writing firmware image to a STM32H7A3AII6Q via internal boot-loader. I'm using AN2606 and AN3155 as reference documents. 
    The boot-loader entry sequence I'm using:
State 1: BOOT0: high

              RST: low

State 2: Wait 200 ms

State 3: BOOT0: high

              RST: high

Then I'm sending 0x7F over USART2 but, getting no response(0x79).

Can you please help me what might be wrong here?

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Dec 24, 2025 2:57 PM UTC

Sorry I have an issue with the notifications today and didn't know you replied to me.

From your oscilloscope screenshot it seems you have that 0x7F which the target is waiting for:

mALLEm_0-1766587829852.png

Meanwhile I still insist on the hardware check:

1- Is there a mean to connect with the STM32H7 with STLINK?, to confirm if the chip is alive?

2- If you can connect with ST-LINK, check again your hardware and continuity between STM32H7_TX / USB-USART_Rx and  STM32H7_RX / USB-USART_Tx. You need to confirm that part and check if you are using the right pins. You could have a mismatch with what you are really doing and what you are thinking about what you did ;).

 

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

8 replies

mƎALLEm
ST Technical Moderator
Dec 24, 2025 9:31 AM UTC

Hello,

You didn't tell what IOs you have used for USART2? PA2 and PA3?

mALLEm_0-1766568617243.png

If yes check your wiring (continuity test). Use an oscilloscope to check what happens on Tx and Rx.

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Associate III
Dec 24, 2025 10:15 AM UTC

The board uses USART2: PA2,PA3. The USART is working well when connected to other boards and running application firmware. But, when isolated and tested by serial, there is no activity on USART: TX in the oscilloscope. 

The USB serial parameters:

BAUD: 115200

PARITY: EVEN

STOP: 1

mƎALLEm
ST Technical Moderator
Dec 24, 2025 10:28 AM UTC

@shubhenduatadben wrote:

The USB serial parameters:

BAUD: 115200

PARITY: EVEN

STOP: 1


You need to check that USB to UART bridge..connect its tx and rx and use an Hyperterminal and check if what you send you receive it. 

And use CubeProgrammer to connect to the ST bootloader: 

mALLEm_0-1766571995294.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
TDK
Dec 24, 2025 2:42 PM UTC

You need to be in the bootloader in order for 0x7F to have an effect. AN2606 lists the ways to enter the bootloader. Most commonly, holding BOOT0 high during reset will enter the bootloader under most circumstances.

"If you feel a post has answered your question, please click ""Accept as Solution""."