Skip to main content
Associate II
Apr 11, 2025 5:09 PM UTC
Solved

STM32H7A3 stuck in SystemClock_Config in KEIL

I have a problem with an STM32H7A3 which remains stuck in SystemClock_Config. I use Keil. Any ideas please?

it just remain stucked here:

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)



void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

/*AXI clock gating */
RCC->CKGAENR = 0xFFFFFFFF;

/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

/** Configure LSE Drive Capability
*/
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE
|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = 64;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 42;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 4;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}

/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
{
Error_Handler();
}
}
This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 11, 2025 6:16 PM UTC

According to what you provided as info, I'm pretty sure it's a hardware issue: broken crystal, crystal not suitable, big value of the serie resistor Rext (if it's available)  or the crystal is not well connected to the MCU pins.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

13 replies

mƎALLEm
ST Technical Moderator
Apr 11, 2025 5:26 PM UTC

Hello @laurianus 

  1. Please use </>  button to format your shared code. See this post. (I'm editing your post).
  2. You need to share your schematics especially the HSE and the LSE parts.
  3. Please don't write to the reserved bits:
    /*AXI clock gating */
    RCC->CKGAENR = 0xFFFFFFFF;

 

mALLEm_1-1744392789747.png

Keep them to 0.

Thanks

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
laurianusAuthor
Associate II
Apr 11, 2025 5:30 PM UTC

It was stuck in LSE so I just changed from LSE to LSI and is working now. Maybe it is a problem with LSE Crystal

mƎALLEm
ST Technical Moderator
Apr 11, 2025 5:37 PM UTC

Most probably the LSE didn't start . In that case you need to review your crystal parameters based on the application AN2867 "Guidelines for oscillator design on STM8AF/AL/S and STM32 MCUs/MPUs".

At first step try to increase the drive level using this macro:

__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

Or your crystal is disconnected from the MCU pins

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Apr 11, 2025 5:49 PM UTC

Where's it stuck? the VOSRDY line?

What board? The NUCLEO-H7A3ZI-Q?

Sure this is an LDO board and not SMPS ?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
laurianusAuthor
Associate II
Apr 11, 2025 5:54 PM UTC

Where's it stuck? the VOSRDY line?

What board? The NUCLEO-H7A3ZI-Q?

Sure this is an LDO board and not SMPS ?


It stuck here

while (__HAL_RCC_GET_FLAG(RCC_FLAG_LSIRDY) == 0U)

It is a custom board and it has LDO power supply

 

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 11, 2025 6:16 PM UTC

According to what you provided as info, I'm pretty sure it's a hardware issue: broken crystal, crystal not suitable, big value of the serie resistor Rext (if it's available)  or the crystal is not well connected to the MCU pins.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.