Skip to main content
GS1
Senior III
Mar 30, 2022 3:06 PM UTC
Solved

STM32H7A3 OctoSPI Memory Mapped Mode Write Problem to HyperRAM S70KL1282

I am struggeling with a HyperRAM on STM32H7A3 with OctoSPI2 in Memory Mapped Mode Write.

In order to check, if the access to the HyperRAM is ok, I am running through a loop which writes all 0 / 0x55555555 / 0xAAAAAAAA (with 32 Bit access) to the RAM and then tests if it is ok. In the debugger memory dump I see that most words are written ok, But almost regularly on the last 4 bytes of a 256 byte block the data is not always written.

Signals are looking good. I tried to reduce clock rate, change the timing parameters, etc. but no success.

Has anybody an idea of what might be wrong?

void MX_OCTOSPI2_Init(void)

{

 /* USER CODE BEGIN OCTOSPI2_Init 0 */

 /* USER CODE END OCTOSPI2_Init 0 */

 OSPIM_CfgTypeDef sOspiManagerCfg = {0};

 OSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};

 /* USER CODE BEGIN OCTOSPI2_Init 1 */

   // 24 = Device 16 MByte Size

   //

   // Prescaler:

   // 3 = 93 MHz 

   // 4 = 70 MHz!

   // 5 = 56 MHz

   // 8 = 35 MHz

   // 16 = 17.5 MHz

   //

 //

 /* USER CODE END OCTOSPI2_Init 1 */

 hospi2.Instance = OCTOSPI2;

 hospi2.Init.FifoThreshold = 4;

 hospi2.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;

 hospi2.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;

 hospi2.Init.DeviceSize = 24;

 hospi2.Init.ChipSelectHighTime = 1;

 hospi2.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;

 hospi2.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;

 hospi2.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;

 hospi2.Init.ClockPrescaler = 5;

 hospi2.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;

 hospi2.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;

 hospi2.Init.ChipSelectBoundary = 23; /* memory die boundary 2^23=8MBs*/

 hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED;

 hospi2.Init.MaxTran = 0;

 hospi2.Init.Refresh = 200;

 if (HAL_OSPI_Init(&hospi2) != HAL_OK)

 {

   Error_Handler();

 }

 sOspiManagerCfg.ClkPort = 2;

 sOspiManagerCfg.DQSPort = 2;

 sOspiManagerCfg.NCSPort = 2;

 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;

 sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_2_HIGH;

 sOspiManagerCfg.Req2AckTime = 1;

 if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

   Error_Handler();

 }

 sHyperBusCfg.RWRecoveryTime = 3;

 sHyperBusCfg.AccessTime = 6;

 sHyperBusCfg.WriteZeroLatency = HAL_OSPI_LATENCY_ON_WRITE;

 sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;

 if (HAL_OSPI_HyperbusCfg(&hospi2, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

   Error_Handler();

 }

S70KL1281_EnableMemoryMappedMode(&hospi2);

}

int32_t S70KL1281_EnableMemoryMappedMode(OSPI_HandleTypeDef *Ctx)

{

 OSPI_HyperbusCmdTypeDef sCommand;

 OSPI_MemoryMappedTypeDef sMemMappedCfg;

 /* OctoSPI Hyperbus command configuration */

 sCommand.AddressSpace = HAL_OSPI_MEMORY_ADDRESS_SPACE;

 sCommand.AddressSize = HAL_OSPI_ADDRESS_32_BITS;

 sCommand.Address     = 0;

 sCommand.DQSMode     = HAL_OSPI_DQS_ENABLE;

 sCommand.NbData      = 1;

 if (HAL_OSPI_HyperbusCmd(Ctx, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)

 {

   return S70KL1281_ERROR;

 }

 /* OctoSPI activation of memory-mapped mode */

 sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;

 if (HAL_OSPI_MemoryMapped(Ctx, &sMemMappedCfg) != HAL_OK)

 {

   return S70KL1281_ERROR;

 }

 return S70KL1281_OK;

}

Thank you for any replies.

Best regards

GS

This topic has been closed for replies.
GS1
GS1Best answer
Senior III
Mar 31, 2022 3:42 PM UTC

Solution for anyone interested:

Set sHyperBusCfg.AccessTime = 7; (instead of 6)

HyperRam now does the job correctly.

2 replies

GS1
GS1AuthorBest answer
Senior III
Mar 31, 2022 3:42 PM UTC

Solution for anyone interested:

Set sHyperBusCfg.AccessTime = 7; (instead of 6)

HyperRam now does the job correctly.

Visitor II
Nov 9, 2023 3:53 PM UTC

Thanks a lot!

This solved my problem of using HyperRAM.