Skip to main content
Joseph.Paul
Associate II
May 1, 2024 5:28 PM UTC
Question

STM32H7A3 External Crystal

can we use internal 24MHz clock for STM32H7A3VIH6Q host or we should use external? Maybe in the future we are going to use USB. Now, just UART and SPI, should I use external to support USB in the future?

This topic has been closed for replies.

1 reply

AScha.3
Super User
May 1, 2024 5:49 PM UTC

For better precision (and low jitter) use external crystal. USB anyway needs it .

I recommend an oscillator (i use also) , no trouble with caps etc. ; today not much more expensive than a crystal and the caps.

And a damping resistor (51r) in the clock line, to avoid ringing.

Something like this: 520-2520MV-160-CNT

https://www.mouser.de/ProductDetail/ECS/ECS-2520MV-160-CN-TR?qs=byeeYqUIh0MIhToPrW09tg%3D%3D

AScha3_0-1714585597830.png

or if you want 24 M  : 520-2520MV-240-BN-T

 

If you feel a post has answered your question, please click on " Best Answer ".