Skip to main content
Associate II
April 16, 2024
Question

STM32H755 I2c BDMA BUSY ON SECOND CALL

  • April 16, 2024
  • 0 replies
  • 472 views

I am having issues with BDMA on consecutive transfers, the DMA handle is always in the busy state on the second call. 

I call this from my application and first transfer works as expected, goes into ISR 

void HAL_I2C_MemRxCpltCallback(I2C_HandleTypeDef *hi2c);

 

HAL_StatusTypeDef HAL_I2C_Mem_Write_DMA(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint16_t MemAddress,
 uint16_t MemAddSize, uint8_t *pData, uint16_t Size)

 

 This call returns error on second transfer because hi2c->hdmatx->State is 

HAL_DMA_STATE_BUSY

 

 dmaxferstatus = HAL_DMA_Start_IT(hi2c->hdmatx, (uint32_t)pData, (uint32_t)&hi2c->Instance->TXDR,
 hi2c->XferSize);

 

 

I call HAL_I2C_Mem_Write_DMA on every transfer and wait for the previous transfer to finish before calling again but still remains busy. Wondering if this is incorrect implementation.

Thanks

This topic has been closed for replies.