Skip to main content
Associate III
November 22, 2024
Question

STM32H753ZI: Can ADC0, ADC1 & ADC2 be sampled simultaneously with same clock?

  • November 22, 2024
  • 4 replies
  • 1033 views

Hi,

1. Can the selected input channels to ADC0, ADC1 and ADC2 in STM32H753ZI be sampled simultaneously under the same sampling clock?

2. NUCLEO-H753ZI ADC does not accept the analog negative signal inputs. Is there any STM32H7 dev board(s) accepting the analog negative signal inputs?

   Thanks,

This topic has been closed for replies.

4 replies

ELABI.1
ST Technical Moderator
November 28, 2024

Hi @RongShengWang 

For the first question: If you want to use this application by using the Injected Simultaneous Mode with Dual ADC, you can refer to the reference manual RM0433, specifically Section 25.4.32 Dual ADC modes. Otherwise, if you want to use 3 ADCs simultaneously, you can use a timer to trigger the 3 ADCs.

For the second question: There are no STM32H7 development boards accepting the analog negative signal inputs.

Thanks,

ELABI.1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate III
November 28, 2024

Thanks, ELABI.1 - Yes, we only want to use all 3 ADCs simultaneously by using a timer to trigger the 3 ADCs.

    ADC 1, 2, 3 have total 60 channels. But only 36 different analog signals are allowed to be connected since there are 16 channels shared by all ADC 1, 2, 3, plus 8 unavailable channels.
    Question: What is the reason to have so many shared channels, which reduces the number of analog signals to be connected?

Thanks

Rong

raptorhal2
Lead
November 28, 2024

What is the reason to have so many shared channels,

My guesses:

1. For more flexibility in assigning channels to multiple ADCs converting at different frequencies.

2. Noise and real estate reduction. Routing to 60 pins would overlap more close proximity digital circuitry and use up more chip space.

Cheers