STM32H753ZI ADC+DMAで高速サンプリングできない。(解決方法の相談)
I am using NUCLEO-H753ZI (STM32H753ZITxLQFP144).
Using ADC1_IN3 Single-ended (PA6) and DMA (Mode:Circular),
I want to perform high-speed sampling. (1MSa/s or more)
Calculated: 3.125MSa/s = 50MHz / 4 * (1.5 + 6.5) (Supplement: clockPrescaler=4, 1.5Cycles, 6.5ADC clock cycles)
*The clock uses 50MHz of PLL2.
However, it seems that the speed is only around 500kSa/s.
Please advise if there are any possible causes or places where the settings may be incorrect.