Skip to main content
XHach.1
Associate
March 10, 2022
Question

STM32H753xI SDMMC data corruption with IDMA and CPU DCACHE enabled

  • March 10, 2022
  • 3 replies
  • 1658 views

Reading blocks from a SD card often result in corrupted data if IDMA and CPU Data Cache are enabled. I am not sure if this falls under erratum 2.1.1 of STM32H753xI. Attached are the STM32Cube project and modified main I used to run tests.

The code in the main reads alternatively the first and second blocks of the SD card and resets the read buffer to 0x55 as a sanity check to verify that internal memory is written. In my test, the connected SD card had a valid FAT32 file system so I knew what data should be read.

Using HAL_SD_ReadBlocks_DMA() to read a block always results in corrupted data while CPU DCACHE is enabled. There is however no corruption if either reading blocks using HAL_SD_ReadBlocks_DMA() when CPU DCACHE is disabled (commenting SCB_EnableDCache() in main.c) or if using HAL_SD_ReadBlocks_IT() / HAL_SD_ReadBlocks() when CPU DCACHE is enabled.

I first encountered this issue in another code base I am working on where it is desired to have CPU DCACHE enabled and use SDMMC IDMA. Is this a real issue or am I missing something?

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
March 10, 2022

>>Is this a real issue or am I missing something?

Cache coherency is a real problem, that *you* have to manage.

You can do it from the MPU configuration.

You can do it with DCache Clean / Invalidate by Address functions.

Perhaps some examples in the FatFs DISKIO DMA code, see

STM32Cube_FW_F7_V1.16.0\Middlewares\Third_Party\FatFs\src\drivers\sd_diskio_dma_template_bspv1.c

#define ENABLE_SD_DMA_CACHE_MAINTENANCE 1

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
mƎALLEm
ST Technical Moderator
March 11, 2022

Hello,

Indeed, this is a data cache coherency issue.

We suggest you to read the AN4839 "Level 1 cache on STM32F7 Series and STM32H7 Series"

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
XHach.1
XHach.1Author
Associate
March 11, 2022

Thanks for the info.