Skip to main content
Associate
Oct 20, 2025 1:35 PM UTC
Solved

STM32H753xI - LCD-TFT controller (LTDC) timing diagram

Hello,

I am reading 6.3.30 LCD-TFT controller (LTDC) section to interface with DS90C385A (LCD) or ADV7125 (VGA)

Assume that LCD Clock (pixel clock) polarity is set to high. Ideally, we can expect rising edge of clock aligned to the middle of the data.  But I can see there is a more time for setup and less time for hold. Refer the figure 46 of datasheet. 

vinoth_ta_0-1760967287789.png

 

 

Note: I am going configure pixel clock low for DS90C385A (LCD) and high for ADV7125 (VGA).  Also, I need to ensure HW work till 150MHz clock. 

 

 

 

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Oct 24, 2025 3:34 PM UTC

Hello @vinoth_ta ;

 

According to the datasheet, the minimum data output hold time is 0ps but the maximum data output hold time is not limited.

KDJEM1_0-1761319387076.png

Thanks to its timings and hardware interface flexibility, the LCD-TFT controller is able to drive several monitors
with different resolutions and signal polarities. There is no risk if you make the correct length matching.  

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

4 replies

KDJEM.1
ST Technical Moderator
Oct 21, 2025 8:01 AM UTC

Hello @vinoth_ta and welcome to the community;

 

According RM0433 Rev 8 Programmable polarity section "The horizontal and vertical synchronization, data enable and pixel clock output signals polarity can be programmed to active high or active low through the LTDC_GCR register"
 In the datasheet section 6.3.30 LCD-TFT controller (LTDC) characteristics, can find measurements of the LTDC characteristics with a specific configuration.

KDJEM1_0-1761033362231.png

 

To use the LTDC, I recommend you to start by looking at Introduction to LCD-TFT display controller (LTDC) on STM32 MCUs - Application note may help you.

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
vinoth_taAuthor
Associate
Oct 24, 2025 11:41 AM UTC

Thanks for your response. I will rewrite my question other way. 

 I am interface STM32 with DS90C385A (LCD). The MCU can have data output hold time th(DATA) of 0 ns. But the chip DS90C385A needs hold time of min 0.5ns. Assume that clock and RGB data length matched to 0 ps delay. 

I am hoping for high chance of timing violation if we do the 0ps length matching. Is it make a sense?

 

 

 

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Oct 24, 2025 3:34 PM UTC

Hello @vinoth_ta ;

 

According to the datasheet, the minimum data output hold time is 0ps but the maximum data output hold time is not limited.

KDJEM1_0-1761319387076.png

Thanks to its timings and hardware interface flexibility, the LCD-TFT controller is able to drive several monitors
with different resolutions and signal polarities. There is no risk if you make the correct length matching.  

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
ST Technical Moderator
Dec 5, 2025 8:55 AM UTC

Hello @vinoth_ta ;

 

Is my reply answer your request?

If you have any further questions, please feel free to ask them.

If your request is answered,  please click on Accept as Solution on the reply which answered your question.

 

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.