Skip to main content
MFäh.1
Associate III
May 2, 2025 1:47 PM UTC
Solved

stm32H753 vs stm32H733

Hi 

I just wanted to ask which of the two processors is actually more powerful. The H733 seems faster, but according to Google AI, the H753 offers better performance :). What’s your take on it?

 

Thank you

BR 

This topic has been closed for replies.
TDK
TDKBest answer
May 2, 2025 1:53 PM UTC

According to objective facts, the H733 is faster and has a larger cache. It will therefore run code faster. I would call that more powerful.

H753: 

  • 480 MHz fCPU/, 2424 CoreMark /1027 DMIPS executing from Flash memory

H733: 

  • 550 MHz fCPU, 2778 CoreMark /1177 DMIPS executing from Flash memory
"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
May 2, 2025 1:53 PM UTC

According to objective facts, the H733 is faster and has a larger cache. It will therefore run code faster. I would call that more powerful.

H753: 

  • 480 MHz fCPU/, 2424 CoreMark /1027 DMIPS executing from Flash memory

H733: 

  • 550 MHz fCPU, 2778 CoreMark /1177 DMIPS executing from Flash memory
"If you feel a post has answered your question, please click ""Accept as Solution""."
MFäh.1
MFäh.1Author
Associate III
May 2, 2025 2:15 PM UTC

Thank you!