Skip to main content
Associate II
August 25, 2025
Solved

STM32H753 SPI Transmission

Hi,

 

I'm using the STM32H753-NUCLEO Board for some SW development, and I'm having some issues with the SPI Handling.

I'm attempting to transmit a single 16-bit data packet, however on the scope I'm transmitting two 16-bit data packets. When I change my data packet type to 8 bits, I'm transmitting 4 8-bit data packets.

I've scoured the RM0433 manual but cannot find the register which tells the peripheral to only transmit a single data packet.

Could someone point me to the correct register and what it should be set to to achieve this please?

This topic has been closed for replies.
TDK
TDKBest answer
August 25, 2025

Use byte or half-word writes to DR, otherwise it does data packing.

// half-word write
*(volatile uint16_t*)&SPIx->TXDR = .;

// byte write
*(volatile uint8_t*)&SPIx->TXDR = .;

 

https://github.com/STMicroelectronics/stm32h7xx-hal-driver/blob/dbfb749f229e1aa89e50b54229ca87766e180d2d/Inc/stm32h7xx_ll_spi.h#L2504

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
August 25, 2025

Use byte or half-word writes to DR, otherwise it does data packing.

// half-word write
*(volatile uint16_t*)&SPIx->TXDR = .;

// byte write
*(volatile uint8_t*)&SPIx->TXDR = .;

 

https://github.com/STMicroelectronics/stm32h7xx-hal-driver/blob/dbfb749f229e1aa89e50b54229ca87766e180d2d/Inc/stm32h7xx_ll_spi.h#L2504

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
August 26, 2025

That's perfect, thank you!