Skip to main content
Visitor II
Mar 25, 2026 10:12 AM UTC
Solved

STM32H753 QUADSPI – Clarification on Dual Bank, IO Lines, and Multi-Flash Possibilities

Hi Team,

I am designing a custom PCB using STM32H753 and planning to use the QUADSPI peripheral for external memory. My use case is data read/write (indirect mode) — not XIP or memory-mapped execution.

While working in STM32CubeMX, I came across some configurations that are confusing, and I’d like to clarify the actual hardware behavior.


1. Dual Bank vs Chip Select behavior

In CubeMX, I can configure:

  • QuadSPI Mode: Dual Bank with Quad Lines

  • Chip Select options:

    • Enable Chip Select 1 for both banks

    • Enable Chip Select 2 for both banks

    • Enable Chip Select for each bank

My understanding:

  • NCS → Bank1

  • NCS2 → Bank2

Questions:

  • If I select “Enable Chip Select 1 for both banks”, does this mean:

    • Only one physical flash is used and banks are logical partitions?

    • Or is there any way two physical memories are still utilized?

  • What is the exact meaning of “bank” in this context (hardware vs logical)?


2. BK1_IOx and BK2_IOx pins confusion

CubeMX exposes:

  • QUADSPI_BK1_IO0–IO3

  • QUADSPI_BK2_IO0–IO3

This gives the impression of 8 data lines (4 per bank).

Questions:

  • Are BK1_IOx and BK2_IOx:

    • Independent data buses for each bank?

    • Or alternate pin mappings of the same internal IO signals?

  • If both sets are enabled simultaneously (as CubeMX allows), are these pins internally shorted?

  • What is the correct way to route these signals on PCB when using:

    • Single flash

    • Dual flash (2-chip setup)


3. Multi-flash usage beyond 2 chips

Given the hardware has:

  • 1 shared IO bus

  • 2 chip select lines (NCS, NCS2)

Questions:

  • Is it possible in any supported way to interface 4 QSPI flash chips

4. Manual Chip Select using GPIO

Questions:

  • Can we use GPIO-controlled chip select instead of the hardware NCS/NCS2 pins in QUADSPI?

  • Or is hardware-controlled CS mandatory for correct operation?

  • If GPIO CS is used:

    • Will timing or protocol issues occur?

    • Is it reliable for read/write (non-memory-mapped mode)?

5. Dual Bank + 1 CS behavior

Questions:

  • In dual bank with single CS configuration, is it possible to:

    • Read/write data to two different physical chips?

    • Or does it always operate on only one physical chip?

  • If it is only one chip, is this configuration purely a logical memory split?


6 Extending dual-bank concept

Questions:

  • If dual bank works with 2 CS lines (2 chips), is there any way to extend this concept to:

    • 4 chips (e.g., 2 banks × 2 chips each)?

  • Can STM32 QUADSPI handle such a setup in any supported or semi-supported way?


7. Summary of my understanding (please correct if wrong)

  • QUADSPI has only one internal 4-bit data bus

  • BK1_IOx and BK2_IOx are not independent buses

  • True multi-chip support is limited to 2 devices via NCS/NCS2

  • “Dual bank with single CS” is logical partitioning, not physical dual memory


I would really appreciate clarification from someone who has worked with this peripheral at hardware level or designed boards using it.

Thanks in advance!

JYOTHISH B CHANDRAN

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 25, 2026 10:49 AM UTC

Hello @jyothzz and welcome to the ST community,

I think the answer to you question has been answered in the AN4760 "Introduction to Quad-SPI interface for STM32 MCUs and MPUs" / Table 9. Dual-Flash hardware configurations:

screenshot.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 25, 2026 10:49 AM UTC

Hello @jyothzz and welcome to the ST community,

I think the answer to you question has been answered in the AN4760 "Introduction to Quad-SPI interface for STM32 MCUs and MPUs" / Table 9. Dual-Flash hardware configurations:

screenshot.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.