STM32H750B-DK not able to program using system workbench
I have purchased STM32H750B-DK. I am using system workbench for stm32 as IDE. Now i downloaded STM32CubeH7 library and trying to download GPIO_IO_Toggle example program into this board but getting the error as below:
17:31:42 **** Programming project XIP_QSPI_InternalSRAM on chip ****
"C:\\Ac6\\SystemWorkbench\\plugins\\fr.ac6.mcu.externaltools.openocd.win32_1.23.0.201904120827\\tools\\openocd\\bin\\openocd.exe" -f stm32.flash.7461493753358478492.cfg -s "D:\\source\\STM32CubeH7\\Projects\\STM32H750B-DK\\Examples\\GPIO\\GPIO_IOToggle\\SW4STM32\\XIP_QSPI_InternalSRAM" -s "C:\\Ac6\\SystemWorkbench\\plugins\\fr.ac6.mcu.debug_2.5.0.201904120827\\resources\\openocd\\st_scripts" -c "program Debug/XIP_QSPI_InternalSRAM.elf verify " -c shutdown
Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 4000 kHz
adapter_nsrst_delay: 100
Info : clock speed 4000 kHz
Info : STLINK v3 JTAG v3 API v3 M2 VID 0x0483 PID 0x374E
Info : using stlink api v3
Info : Target voltage: 3.290245
Info : Unable to match requested speed 4000 kHz, using 3300 kHz
Info : Stlink adapter speed set to 3300 kHz
Info : STM32H750XBHx.cpu0: hardware has 8 breakpoints, 4 watchpoints
Info : Listening on port 3333 for gdb connections
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x080002d8 msp: 0x20020000
Info : Unable to match requested speed 4000 kHz, using 3300 kHz
Info : Stlink adapter speed set to 3300 kHz
Info : Unable to match requested speed 4000 kHz, using 3300 kHz
adapter speed: 3300 kHz
** Programming Started **
auto erase enabled
Info : Device: STM32H7xx 2M
Info : flash size probed value 128
Info : STM32H flash size is 128kb, base address is 0x8000000
Warn : no flash bank found for address 90000000
Warn : no flash bank found for address 90001190
wrote 0 bytes from file Debug/XIP_QSPI_InternalSRAM.elf in 0.006981s (0.000 KiB/s)
** Programming Finished **
** Verify Started **
Error: timed out while waiting for target halted
target halted due to debug-request, current mode: Handler HardFault
xPSR: 0x81000003 pc: 0x080009ce msp: 0x2001ffe0
Error: error executing cortex_m crc algorithm
Error: checksum mismatch - attempting binary compare
diff 0 address 0x90000000. Was 0x11 instead of 0x00
diff 1 address 0x90000002. Was 0x00 instead of 0x02
diff 2 address 0x90000003. Was 0x00 instead of 0x20
diff 3 address 0x90000004. Was 0x00 instead of 0x45
diff 4 address 0x90000005. Was 0x10 instead of 0x0f
diff 5 address 0x90000008. Was 0x00 instead of 0x07
diff 6 address 0x90000009. Was 0x00 instead of 0x11
diff 7 address 0x9000000b. Was 0x00 instead of 0x90
diff 8 address 0x9000000c. Was 0xc0 instead of 0x09
diff 9 address 0x9000000d. Was 0x5d instead of 0x11
diff 10 address 0x9000000f. Was 0x00 instead of 0x90
diff 11 address 0x90000010. Was 0x40 instead of 0x0b
diff 12 address 0x90000011. Was 0x1f instead of 0x11
diff 13 address 0x90000013. Was 0x00 instead of 0x90
diff 14 address 0x90000014. Was 0xe4 instead of 0x0d
diff 15 address 0x90000015. Was 0x0c instead of 0x11
diff 16 address 0x90000017. Was 0x00 instead of 0x90
diff 17 address 0x90000018. Was 0xe8 instead of 0x0f
diff 18 address 0x90000019. Was 0x03 instead of 0x11
diff 19 address 0x9000001b. Was 0x00 instead of 0x90
diff 20 address 0x9000001c. Was 0xc8 instead of 0x00
diff 21 address 0x90000020. Was 0x32 instead of 0x00
diff 22 address 0x90000024. Was 0x05 instead of 0x00
diff 23 address 0x9000002c. Was 0x00 instead of 0x95
diff 24 address 0x9000002d. Was 0x00 instead of 0x0f
diff 25 address 0x9000002f. Was 0x00 instead of 0x90
diff 26 address 0x90000030. Was 0x00 instead of 0x11
diff 27 address 0x90000031. Was 0x00 instead of 0x11
diff 28 address 0x90000033. Was 0x00 instead of 0x90
diff 29 address 0x90000038. Was 0x00 instead of 0x95
diff 30 address 0x90000039. Was 0x00 instead of 0x0f
diff 31 address 0x9000003b. Was 0x00 instead of 0x90
diff 32 address 0x9000003c. Was 0x00 instead of 0x13
diff 33 address 0x9000003d. Was 0x00 instead of 0x11
diff 34 address 0x9000003f. Was 0x00 instead of 0x90
diff 35 address 0x90000040. Was 0x00 instead of 0x95
diff 36 address 0x90000041. Was 0x00 instead of 0x0f
diff 37 address 0x90000043. Was 0x00 instead of 0x90
diff 38 address 0x90000044. Was 0x00 instead of 0x95
diff 39 address 0x90000045. Was 0x00 instead of 0x0f
diff 40 address 0x90000047. Was 0x00 instead of 0x90
diff 41 address 0x90000048. Was 0x00 instead of 0x95
diff 42 address 0x90000049. Was 0x00 instead of 0x0f
diff 43 address 0x9000004b. Was 0x00 instead of 0x90
diff 44 address 0x9000004c. Was 0x00 instead of 0x95
diff 45 address 0x9000004d. Was 0x00 instead of 0x0f
diff 46 address 0x9000004f. Was 0x00 instead of 0x90
diff 47 address 0x90000050. Was 0x00 instead of 0x95
diff 48 address 0x90000051. Was 0x00 instead of 0x0f
diff 49 address 0x90000053. Was 0x00 instead of 0x90
diff 50 address 0x90000054. Was 0x00 instead of 0x95
diff 51 address 0x90000055. Was 0x00 instead of 0x0f
diff 52 address 0x90000057. Was 0x00 instead of 0x90
diff 53 address 0x90000058. Was 0x00 instead of 0x95
diff 54 address 0x90000059. Was 0x00 instead of 0x0f
diff 55 address 0x9000005b. Was 0x00 instead of 0x90
diff 56 address 0x9000005c. Was 0x00 instead of 0x95
diff 57 address 0x9000005d. Was 0x00 instead of 0x0f
diff 58 address 0x9000005f. Was 0x00 instead of 0x90
diff 59 address 0x90000060. Was 0x00 instead of 0x95
diff 60 address 0x90000061. Was 0x00 instead of 0x0f
diff 61 address 0x90000063. Was 0x00 instead of 0x90
diff 62 address 0x90000064. Was 0x00 instead of 0x95
diff 63 address 0x90000065. Was 0x00 instead of 0x0f
diff 64 address 0x90000067. Was 0x00 instead of 0x90
diff 65 address 0x90000068. Was 0x00 instead of 0x95
diff 66 address 0x90000069. Was 0x00 instead of 0x0f
diff 67 address 0x9000006b. Was 0x00 instead of 0x90
diff 68 address 0x9000006c. Was 0x00 instead of 0x95
diff 69 address 0x9000006d. Was 0x00 instead of 0x0f
diff 70 address 0x9000006f. Was 0x00 instead of 0x90
diff 71 address 0x90000070. Was 0x00 instead of 0x95
diff 72 address 0x90000071. Was 0x00 instead of 0x0f
diff 73 address 0x90000073. Was 0x00 instead of 0x90
diff 74 address 0x90000074. Was 0x00 instead of 0x95
diff 75 address 0x90000075. Was 0x00 instead of 0x0f
diff 76 address 0x90000077. Was 0x00 instead of 0x90
diff 77 address 0x90000078. Was 0x00 instead of 0x95
diff 78 address 0x90000079. Was 0x00 instead of 0x0f
diff 79 address 0x9000007b. Was 0x00 instead of 0x90
More than 128 errors, the rest are not printed.
embedded:startup.tcl:476: Error: ** Verify Failed **
in procedure 'program'
in procedure 'program_error' called at file "embedded:startup.tcl", line 521
at file "embedded:startup.tcl", line 476
17:32:03 Build Finished (took 20s.731ms)
Any help would be highly appreciated.