STM32H750: Cannot run IWDG1 Watchdog
Somehow my IWDG1 does not start. I follow exactly the instruction in the manual:
IWDG1->KR= (DWORD)0xcccc; // Start IWDG
IWDG1->KR= (DWORD)0x5555; // Access registers IWDG
IWDG1->PR= 0;
IWDG1->RLR= 500;
... but if I check now IWDG1->SR, then the RUV Bit keeps on 1, and the
RLR register keeps on the reset value 0xFFF (it does NOT change to the specified value of 500). The LSI switches on, as I
see it in RCC->CSR (I also tried already to switch on LSI "manually" first,
but it does not help)
Am I missing here some special trick to start IWDG? (from LSION it seems to start, but RLR does not change...)
The option byte "IWDG_SW" is set, as I see it in ST-Link. Also the bit IWDG_SW in the register FLASH->OPTSR_CUR is set. (I did not change any option bytes so far, this just seems to be the state "as delivered", chip is STM32H750 Version Y).
But strangely in SYSCFG->UR11 the bit IWDGM reads zero... .
The WWDG works ... .
Any help available?