Associate III
August 7, 2023
Question
stm32h747i-disco uart8 transmitir error
- August 7, 2023
- 2 replies
- 975 views
When i use uart8 for send data to arduino(add function in food recognition in the fp_vision_AI) ,when i use MX_USART8_UART_Init();(if i use // jump over this line the rest could run normally) the screen on the board get blocked(stopped),how could i check where i get wrong? anexo this parte of code.
Data i want to send as tipo of "%s %.0f%%"
sprintf(msg, "%s %.0f%%", NN_OUTPUT_CLASS_LIST[App_Context_Ptr->ranking[i]], *((float*)(App_Context_Ptr-;
HAL_UART_Transmit(&huart8,msg,10,1000);