Skip to main content
Associate
Nov 1, 2026 10:46 PM UTC
Solved

STM32H745ZIT3 VCAP voltage issue

Hello, I am in the process of bringing up a custom board integrating an STM32H745ZIT3. The chip is running with VDD at 1.8V and we plan to use LDO only mode for supplying the core. We have assembled our power delivery and MCU on the board, but we are having trouble when powering the board. We see that VCAP reached 1V briefly (for about 4 ms) before seemingly shutting off. The chip is unresponsive to flashing as well. The scope trace below shows VCAP (green) and the NRST signal (yellow).

Below is the relevant part of our schematic. 

We are unsure if we are encountering an issue with our design or if we have an assembly issue causing our board to be non-functional. Please let us know if we can provide any more information to clarify our situation!

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 2, 2026 8:27 AM UTC

Hello ​@Michal Dudka and welcome to the ST community,

What power mode you’ve set in the software? it should be set to LDO nothing else.

If you are using CubeMx, this is what you should set as config:

If you are using directly the HAL you must set the define in your project config: USE_PWR_LDO_SUPPLY

Otherwise you’ve locked you MCU and you need to unlock it by referring to these articles:

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

Michal Dudka
Lead
Nov 2, 2026 7:04 AM UTC

If you've already uploaded a program there, then LDO is probably turned off. See http://www.efton.sk/STM32/gotcha/g201.html

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 2, 2026 8:27 AM UTC

Hello ​@Michal Dudka and welcome to the ST community,

What power mode you’ve set in the software? it should be set to LDO nothing else.

If you are using CubeMx, this is what you should set as config:

If you are using directly the HAL you must set the define in your project config: USE_PWR_LDO_SUPPLY

Otherwise you’ve locked you MCU and you need to unlock it by referring to these articles:

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
nevenAuthor
Associate
Nov 2, 2026 3:31 PM UTC

Yes, you are both correct. We determined last night that this was the issue and managed to erase the program from the board by tying BOOT0 high temporarily. it would be helpful if CubeMX prompted you about this option rather than choosing a default that can brick your MCU.

mƎALLEm
ST Technical Moderator
Nov 2, 2026 3:39 PM UTC

Hello ​@neven ,

If your question has been answered please select one of the above replies that answered your question.

I’ve already escalated for this request change internally.

See this post: 

Hope it will be implemented soon.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.