Skip to main content
Associate
December 26, 2024
Question

STM32H745ZIT3 FMC-NAND Flash IS34_35ML04G081 data corrupted

I am using stm32h745zit3, with the flash is IS34_35ML04G081. I have initialize the below parameter but after writing in to the flash and reading the data but some bytes are corrupted. Please help to resolve this issue.
uint8_t buffer[2048] = {0};

int main(void)
{
 // Initialize the HAL Library and reset all peripherals
 HAL_Init();

 // Configure the system clock
 SystemClock_Config();

 // Initialize FMC (Flexible Memory Controller)
 FMC_Init();

 for (int i = 0, j = 0; i < 2048; i++)
 {
 buffer[j] = j++;
 if (j > 100)
 j = 0;
 }

 while (1)
 {
 HAL_NAND_Write_Page_8b(&hnand1, Address, writeBuff, 1);
 LL_mDelay(1000);
 HAL_NAND_Read_Page_8b(&hnand1, &writeAddress, downloadBff1, 1);
 LL_mDelay(1000);
 }
}

/*******************************************************************************
 * Function Name : SystemClock_Config
 * Description : System Clock Configuration
 * Configures clocks, PLL, and related peripherals.
 * Input : None
 * Output : None
 * Return : None
 ******************************************************************************/
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 // Supply configuration update enable
 HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);

 // Configure the main internal regulator output voltage
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);

 // Wait until voltage scaling flag is ready
 while (!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY))
 {
 }

 // Macro to configure the PLL clock source
 __HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure. */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 2;
 RCC_OscInitStruct.PLL.PLLN = 66;
 RCC_OscInitStruct.PLL.PLLP = 2;
 RCC_OscInitStruct.PLL.PLLQ = 17;
 RCC_OscInitStruct.PLL.PLLR = 2;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
 RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 // Initialization Error
 Error_Handler();
 }

 // Peripheral clock enable
 __HAL_RCC_FMC_CLK_ENABLE();

 // Initialize peripheral clock for FMC
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_FMC;
 PeriphClkInitStruct.PLL2.PLL2M = 2;
 PeriphClkInitStruct.PLL2.PLL2N = 21;
 PeriphClkInitStruct.PLL2.PLL2P = 2;
 PeriphClkInitStruct.PLL2.PLL2Q = 4;
 PeriphClkInitStruct.PLL2.PLL2R = 2;

 PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_3;
 PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOMEDIUM;
 PeriphClkInitStruct.FmcClockSelection = RCC_FMCCLKSOURCE_PLL2;

 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 // Initialization Error */
 Error_Handler();
 }

 /** Initializes the peripherals clock
 * For the USB_FS pphl */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB;
 PeriphClkInitStruct.PLL3.PLL3M = 4;
 PeriphClkInitStruct.PLL3.PLL3N = 32;
 PeriphClkInitStruct.PLL3.PLL3P = 2;
 PeriphClkInitStruct.PLL3.PLL3Q = 4;
 PeriphClkInitStruct.PLL3.PLL3R = 2;
 PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL3VCIRANGE_2;
 PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
 PeriphClkInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_PLL3;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 // Initialization Error
 Error_Handler();
 }

 // Initializes the CPU, AHB and APB buses clocks
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_D3PCLK1 | RCC_CLOCKTYPE_D1PCLK1;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
 RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 // Initialization Error
 Error_Handler();
 }

 // Configure MCO output
 HAL_RCC_MCOConfig(RCC_MCO1, RCC_MCO1SOURCE_HSE, RCC_MCODIV_1);

 // activate CSI clock (required for I/O Compensation Cell)
 __HAL_RCC_CSI_ENABLE();

 // Enable SYSCFG clock (required for I/O Compensation Cell)
 __HAL_RCC_SYSCFG_CLK_ENABLE();

 // Enables the I/O Compensation Cell
 HAL_EnableCompensationCell();
}

/*******************************************************************************
 * Function Name : FMC_Init
 * Description : Initialize the FMC (Flexible Memory Controller) for NAND
 * memory access.
 * This function sets up the controller for NAND flash operations.
 * Input : None
 * Output : None
 * Return : None
 ******************************************************************************/
void FMC_Init(void)
{
 // USER CODE BEGIN FMC_Init 0

 FMC_NAND_PCC_TimingTypeDef ComSpaceTiming = {0}; // Common space timing structure
 FMC_NAND_PCC_TimingTypeDef AttSpaceTiming = {0}; // Attribute space timing structure

 // Initialize the NAND1 memory
 hnand1.Instance = FMC_NAND_DEVICE;

 // hnand1.Init: Configuring NAND bank and settings
 hnand1.Init.NandBank = FMC_NAND_BANK3;
 hnand1.Init.Waitfeature = FMC_NAND_WAIT_FEATURE_DISABLE;
 hnand1.Init.MemoryDataWidth = FMC_NAND_MEM_BUS_WIDTH_8;
 hnand1.Init.EccComputation = FMC_NAND_ECC_DISABLE;
 hnand1.Init.ECCPageSize = FMC_NAND_ECC_PAGE_SIZE_256BYTE;
 hnand1.Init.TCLRSetupTime = TCLRSETUPtIME;
 hnand1.Init.TARSetupTime = TARSETUPTIME;

 // hnand1.Config: NAND memory configuration settings
 hnand1.Config.PageSize = 2048; // Page size
 hnand1.Config.SpareAreaSize = 64; // Spare area size
 hnand1.Config.BlockSize = 64; // Number of pages in a block
 hnand1.Config.BlockNbr = 4096; // Total number of blocks
 hnand1.Config.PlaneNbr = 2; // Number of planes
 hnand1.Config.PlaneSize = 2048; // Size of each plane
 hnand1.Config.ExtraCommandEnable = ENABLE;

 // Configure common space timing
 ComSpaceTiming.SetupTime = 2;
 ComSpaceTiming.WaitSetupTime = 4;
 ComSpaceTiming.HoldSetupTime = 2;
 ComSpaceTiming.HiZSetupTime = 4;

 // Attribute space timing mirrors common space timing
 AttSpaceTiming.SetupTime = ComSpaceTiming.SetupTime;
 AttSpaceTiming.WaitSetupTime = ComSpaceTiming.WaitSetupTime;
 AttSpaceTiming.HoldSetupTime = ComSpaceTiming.HoldSetupTime;
 AttSpaceTiming.HiZSetupTime = ComSpaceTiming.HiZSetupTime;

 // Initialize the NAND interface and check the result
 if (HAL_NAND_Init(&hnand1, &ComSpaceTiming, &AttSpaceTiming) != HAL_OK)
 {
 // Initialization Error
 Error_Handler();
 }
}
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
December 27, 2024

Your code looks incomplete, buffer initialization look sketchy

Perhaps start by doing one, instrument the code some via a serial console, show the delta between expected.

Does it need an Erase? Check the initialization. Pull some data sheets, and do some debugging.

https://www.issi.com/WW/pdf/IS34_35ML04G081.pdf

Probably very few with your part choice or hardware, you'll probably need to own this.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
rahul8878Author
Associate
December 28, 2024

I have initiated with

uint8_t downloadBff1[2112] = "", writeBuff[2112] = "";

WriteAddress and

If starting of the block (0th page) I am using erase.

Then also same issue is coming