Skip to main content
SUzun.1
Associate
April 13, 2020
Question

STM32H745ZI - Reset ONLY CPU2

  • April 13, 2020
  • 0 replies
  • 464 views

Hello!

I want to use CPU1 (CM7) doing the following:

1) Hold CPU2 (CM4)

2) Flash new firmware for CPU2

3) Reset and release CPU2.

During this process CPU1 must be able to keep communicating to a Host via Ethernet / lwip.

______________________________

I can make CPU2 stop by using HSEM notification callbacks like this.

// CPU1 sends notification to CPU2
 
HAL_HSEM_FastTake(HSEM_ID_0);
HAL_HSEM_Release(HSEM_ID_0, 0);
// CPU2 receives notification from CPU1 and enters STOP Mode
 
void HAL_HSEM_FreeCallback(uint32_t SemMask) 
{
	HAL_PWREx_ClearPendingEvent();
	HAL_PWREx_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFE,
	PWR_D2_DOMAIN);
}

I would continue using the HAL Flash libraries to flash new firmware for CPU2 using CPU1.

But how do i reset CPU2 after flashing its firmware using CPU1?

I'm pretty stuck and not sure if this is the way to go.

Thanks for any advices!

Best regards

ser_u

This topic has been closed for replies.