Skip to main content
Associate
Mar 26, 2024 11:52 AM UTC
Solved

STM32H745 set CM7 boot addr0 from CM4

I'm using a STM32H745 and running a bootloader on the CM4. In the bootloader I want to set the boot address of the CM7 using the user option bytes. 

Is this possible and if so, how should I do this?

Kind regards

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 27, 2024 1:06 PM UTC

You're missing:

 

OBInit.BootConfig = OB_BOOT_ADD0;

This sequence is working well from CM4 side:

 

 HAL_FLASH_Unlock();
 HAL_FLASH_OB_Unlock();
 HAL_FLASHEx_OBGetConfig(&OBInit);
	
 OBInit.OptionType = OPTIONBYTE_CM7_BOOTADD;
 OBInit.BootAddr0 = 0x08010000;
 OBInit.BootConfig = OB_BOOT_ADD0;
 HAL_FLASHEx_OBProgram(&OBInit);
 HAL_FLASH_OB_Launch()
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

3 replies

mƎALLEm
ST Technical Moderator
Mar 26, 2024 12:30 PM UTC

I don't see a constraint to do that.

How to modify an option byte? refer to the RM0399 / section 4.4.3 Option byte modification.

An example how to modify option byte is provided here for Flash BANK swapping example.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Sander-WAuthor
Associate
Mar 26, 2024 3:32 PM UTC

I'm using the following to set the boot address for the M7 core from the M4 core application. But somehow the boot address remains the same. Any suggestions?

{
	FLASH_OBProgramInitTypeDef OB;
	HAL_FLASHEx_OBGetConfig(&OB);

	OB.OptionType = OPTIONBYTE_CM7_BOOTADD;
	OB.BootAddr0 = 0x08010000;

	HAL_FLASH_Unlock();
	HAL_FLASH_OB_Unlock();

	if ( HAL_FLASHEx_OBProgram(&OB) != HAL_OK )
	{
		return ;
	}

	HAL_FLASH_OB_Launch();
}
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Mar 27, 2024 1:06 PM UTC

You're missing:

 

OBInit.BootConfig = OB_BOOT_ADD0;

This sequence is working well from CM4 side:

 

 HAL_FLASH_Unlock();
 HAL_FLASH_OB_Unlock();
 HAL_FLASHEx_OBGetConfig(&OBInit);
	
 OBInit.OptionType = OPTIONBYTE_CM7_BOOTADD;
 OBInit.BootAddr0 = 0x08010000;
 OBInit.BootConfig = OB_BOOT_ADD0;
 HAL_FLASHEx_OBProgram(&OBInit);
 HAL_FLASH_OB_Launch()
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.