Skip to main content
HKapo.2
Associate II
July 26, 2024
Solved

STM32H745 freertos lwip simple web server POST Method issue

Hello All,

I have implemented a simple Web server using https://github.com/STMicroelectronics/STM32CubeF7/tree/master/Projects/STM32756G_EVAL/Applications/LwIP/LwIP_HTTP_Server_Socket_RTOS example.

 

The Get method works fine but as soon as I use the POST method I get "The connection was reset" message in my web browser.

 

I am not too famuliar with http protocol so not sure of POST method needs to be treated differently. Below is just sime snip of the code

 

 

 

static void http_server_serve(struct netconn *conn) 
{
static void http_server_serve(struct netconn *conn) 
{
.
.
.

if ((buflen >=5) && (strncmp(buf, "GET /", 5) == 0))
{
/* Check if request to get ST.gif */ 
	if (strncmp((char const *)buf,"GET /STM32F7xx_files/ST.gif",27)==0)
	{
	 fs_open(&file, "/STM32F7xx_files/ST.gif"); 
	 netconn_write(conn, (const unsigned char*)(file.data), (size_t)file.len, NETCONN_NOCOPY);
	 fs_close(&file);
	} 
.
.
.
}
else if ((buflen >=6) && (strncmp(buf, "POST /", 6) == 0))
{
	if (strncmp(buf, "POST /submit", 12) == 0) 
	{
			// Find the start of the request body
			char *body = strstr(buf, "\r\n\r\n");
			if (body != NULL) 
			{
				body += 4; // Skip the \r\n\r\n

				// Extract Content-Length from headers
				char *content_length_str = strstr(buf, "Content-Length:");
				int content_length = 0;
				if (content_length_str != NULL) {
						sscanf(content_length_str, "Content-Length: %d", &content_length);
				}

				// Handle the POST request with dynamic memory allocation
				handle_post_request(conn, body, content_length);
			}	
		}

				 /* Close the connection (server closes in HTTP) */
 netconn_close(conn);
 
 /* Delete the buffer (netconn_recv gives us ownership,
 so we have to make sure to deallocate the buffer) */
 netbuf_delete(inbuf);
}		

void handle_post_request(struct netconn *conn, char *request_body, int content_length) {
{
 const char *response = "HTTP/1.0 201 OK\r\nContent-Type: text/html\r\n\r\n"
 "<html><body>Form submitted successfully</body></html>";
													 
		
 netconn_write(conn, response, strlen(response), NETCONN_COPY);
}

 

 

 

 

Any guidance to guide me is deeply appreciated.

 

This topic has been closed for replies.
LCE
LCEBest answer
Principal III
August 5, 2024

Just wanted to add:

check lwip's httpd, POST is "prepared".

Google for lwip POST example, there's something almost usable for http_post_finished and other functions.

6 replies

Andrew Neil
Super User
July 26, 2024

@HKapo.2 wrote:

I have implemented a simple Web server using https://github.com/STMicroelectronics/STM32CubeF7/tree/master/Projects/STM32756G_EVAL/Applications/LwIP/LwIP_HTTP_Server_Socket_RTOS example.


Does that claim to support POST ?

 


@HKapo.2 wrote:

The Get method works fine but as soon as I use the POST method ...


What are you using to issue those requests?

 


@HKapo.2 wrote:

I am not too familiar with http protocol


Start here: https://www.jmarshall.com/easy/http/

About POST, specifically: https://www.jmarshall.com/easy/http/#postmethod 

Also, tools like curl and wget are good for testing & gaining familiarity ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
HKapo.2
HKapo.2Author
Associate II
July 26, 2024

Thanks Andrew for quick response.

 

I have used packet sender to ensure that a response to Post is being received.

HKapo2_0-1722003673664.png

But when I try submiting the form via web browser I get "The connection was reset" error.

 

Thanks for the link, I will go through it

 

 

 

 

Andrew Neil
Super User
July 26, 2024

The example does say simple Web server.

So maybe its response is just sufficient to be valid as far as the protocol is concerned, but not enough to give the full interaction that your browser is expecting?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
LCE
LCEBest answer
Principal III
August 5, 2024

Just wanted to add:

check lwip's httpd, POST is "prepared".

Google for lwip POST example, there's something almost usable for http_post_finished and other functions.

HKapo.2
HKapo.2Author
Associate II
August 6, 2024

Thanks for the suggestions.

 

I got everyting up and running now.