Skip to main content
DMast.1
Associate III
Dec 17, 2020 2:01 PM UTC
Question

STM32H745 and SPI + DMA

Hi to all,

I need to send on every TIM interrupt a packet stream to SPI1. I can't use the HAL_SPI_Transmit(...) because it is blocking....so I need to use the DMA but not in circular mode.

I can not use the synchronization of DMA with lptim using DMAMUX because I just use all lptim in othe functions. What I need is send on everery TIM isr a packet stream to SPI using DMA but is I use the isr code attached only the first byte get out.

void TIM2_IRQHandler(void)
{
 U16 zDacValue;
 static U8 yDacChannel = Dac2666_eChannel0;
 
 /* Clear interrupt flazOutValuegs */
 __HAL_LPTIM_CLEAR_FLAG(&gLptim3Handle, LPTIM_IT_ARRM);
 yDacChannel++;
 if( yDacChannel >= (sizeof(gDac2Config)/sizeof(Dac2666_tSeqConfig)))
 {
 yDacChannel = 0;
 }
 zDacValue = gDac2Config[yDacChannel].DataBuffer[0];
 
 /* Prepare command for next channel */
 gDac2TxBuffer[0] = gDac2Config[yDacChannel].AdcChannel + (DAC2666_WR_CODE_TO_CHANNEL << 4);
 gDac2TxBuffer[1] = (U8)((zDacValue >> 8) & 0x00FF);
 gDac2TxBuffer[2] = (U8)((zDacValue >> 0) & 0x00FF);
 
 /* Init the SPI interface to ADC converter */
 if( HAL_SPI_Transmit_DMA(GetSpiHandle(HalSpi_eCh1), (U8*)gDac2TxBuffer, DAC2666_SPI_BUFFSIZE) != HAL_OK )
 {
 yDacChannel = 0;
 }
}

This topic has been closed for replies.