STM32H743ZI2 CAN message receive issue with MCP2551
- 3 replies
- 1527 views
I have hooked up a STM32H743ZI2 Nucleo board with a CAN tranceiver MCP2551 following the instructions kindly provided by mr. Hudak (https://os.mbed.com/users/hudakz/code/CAN_Hello/) with the exception of replacing the second board with a USB-CAN-module and sending responses from the pc.
This setup sends CAN messages just fine but doesn't seem to be able to receive the messages sent to the STM board as the attached interrupt event function is never called. Attached is a screenshot of the CAN and serial traffic. By examining the RX pin with oscilloscope I have determined the voltage levels to be sensible and the message is sent from the MCP2551 to the RX pin.
Could this be a problem with the setup of pin interrupts or am I missing some other additional steps that must be taken to set up MCP2551 to work with the STM32H7 board?