Skip to main content
GHARI.1
Associate III
October 2, 2021
Solved

STM32H743ZI Direct channels for ADC.

Hi,

I am using STM32H743ZI micro controller of LQFP144 package. My doubt is that in the data sheet they are mentioning that it has 2 direct channels for ADC but they are not mentioning what are the channels or pins offering this

They are only talking about TFBGA240 +25 package pins offering this direct concept then what about LQFP-144 pins offering this.

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
October 3, 2021

. Direct channels are connected to analog I/Os (PA0_C, PA1_C, PC2_C and PC3_C) to optimize ADC performance

1 reply

MM..1
MM..1Best answer
Super User
October 3, 2021

. Direct channels are connected to analog I/Os (PA0_C, PA1_C, PC2_C and PC3_C) to optimize ADC performance