Skip to main content
Associate III
Jun 17, 2025 2:20 PM UTC
Question

stm32h743zi DFSDM configuration in CubeMX

How do I configure the DFDSM peripheral using CubeMX?

I do know about the application note AN4990 and have read it. I also saw this thread

https://community.st.com/t5/stm32cubemx-mcus/stm32h753-stpms2l-dfsdm-pt100-example-using-stm32cubemx/td-p/172652

and have looked at the example in the stm32cubeh7 firmware repository, but I does not contain the CubeMX .ioc

Is there any example or tutorial?

This topic has been closed for replies.

2 replies

ST Technical Moderator
Jun 17, 2025 2:59 PM UTC

Hello @mo_krauti ,

May this guide AN5027 help you with examples of DFSDM configuration based on STM32CubeMX.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
mo_krautiAuthor
Associate III
Jun 18, 2025 12:01 PM UTC

Thank you for your answer.

I forgot to mention that I have also read AN5027. I have trouble setting up the DMA transfer. How big does the buffer need to be? For now I only want to do one conversion, but in the future it will be about 6.