Skip to main content
Associate III
Aug 22, 2025 8:30 AM UTC
Solved

[STM32H743XGH6] Flash memory

I believe the STM32H743XGH6 has 1 MB of internal flash memory. However, using STM32CubeProgrammer, I was able to write and read data to the reserved area at 0x8180 0000. Is it okay to use this area?

The built-in Flash Memory areas of the STM32H743XGH6 are recognized as
0x8100 0000-0x817F FFFF and 0x8000 0000-0x0801 FFFF.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Aug 22, 2025 9:08 AM UTC

Hello,

This zone of Flash is physically available but not tested in production so its usage is not guaranteed: its usage is  NOT recommended.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Aug 22, 2025 9:08 AM UTC

Hello,

This zone of Flash is physically available but not tested in production so its usage is not guaranteed: its usage is  NOT recommended.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.