Question
STM32H743IIT6: Is an external connection between VCAP1 and VCAP2 required?
Hello ST support,
I am reviewing a PCB design using the STM32H743IIT6 (LQFP176) with its internal LDO enabled.
My current connections are:
- VCAP1, pin 81: a dedicated 2.2 µF ceramic capacitor to VSS.
- VCAP2, pin 125: a separate dedicated 2.2 µF ceramic capacitor to VSS.
- Each capacitor is placed close to its corresponding VCAP pin.
- There is no external connection between VCAP1 and VCAP2.
AN4938 Rev. 7, Section 2.2, page 12 states:
“Connect VCAP1 pin to VCAP2 pin.”
AN4938 hardware development guide
My existing boards(H743VIT6) without this external connection have been operating normally. Before manufacturing the new PCB, I would like to confirm:
- Is connecting VCAP1 and VCAP2 externally required for guaranteed operation, or is it a recommended layout practice?
- Are these pins internally connected? If so, why is the external connection also specified?
- If the external connection is required, are there any specific routing recommendations while keeping both capacitors close to their respective pins?
Thank you for your clarification.